Posted on September 21, 2005 at 11:13Error Correction? Well, I am using the old Hamming code. The amount of hamming bits to be used is up to you to decide... But there is a class of FEC codes called TURBO CODES that are much more efficient, but they...
Posted on April 06, 2005 at 11:46I understood, but you still need at least two wires! :o Remember the communication clock? (CLR/T) :-] regards, Rafael Krapf BRASIL
Posted on April 05, 2005 at 10:48Hi Alok, I am forced to agree with you. TIME TO MARKET IS KILLING. :o :o :o :o Cortex: how did you manage to use only one wire??? how do you say to the ST7538 to transmit and receive? how do you transmit and receive...
Posted on April 04, 2005 at 10:42Hi Alok, sometimes it is not only a matter of solution available, but also infrastructure for munufacturing the product with that device. If our friend already has structure, tools, etc for PIC, why should he use ano...