Posted on May 17, 2011 at 12:01 Thank you all !!!!! sjo you are right! the mistake was in the .VM line!! the PIO bit was enabled!! Thank you very much for helping me!!! Best regards DANIEL
Posted on May 17, 2011 at 12:01Hello! I read the Manual and i've done what your had written! but do not work at all? May be there could be a problem with the PSDsoft project! I'd copied from the USP-Example and had set the PA - Ports to GP I/O!!! No...
Posted on May 17, 2011 at 12:01Hello Forum-Members! I've got a Problem with using the Ports PA0-PA7 at the uPSD3200 - Development Board! At my PSDsoft Express Project i've declareted this Ports to GP I/O Mode. And the Problem is if i want to set a P...
Posted on May 17, 2011 at 12:01HI! I've got a simple question! I think it's easy to solve! sorry! but how could i, for example set a port with using C-code! It's very easy to use PSD Express. But, if i want to write it C what must i do? for example ...
Posted on May 17, 2011 at 12:01 Hello, I 've downloaded the curruent USB_Demo and it work really fine! But now i want to modify a couple of things that i could use it for my purposes. My Problem is the 'vcl.h' isn't surported in the ...