Posted on May 17, 2011 at 12:10There does not appear to be a form for the PSD memories but can you tell me if the SDP ( Software data proection ) is applied for the whole device or does it apply sector by sector. I have tried to protect 2 sectors an...
Posted on May 17, 2011 at 12:08When the PWM is stopped, is there a way of setting the ''OFF'' value of the output pin. I have tried to configure the registers without the clock to set the value without success Thanks
Posted on May 17, 2011 at 12:02I have noticed on my board and the dk300 development that the address lines (AD7-0) Have a the system clock divided by a factor of 4 or 8 continulsly running. Even when the address lines are exercised the clock runs ov...
Posted on May 17, 2011 at 12:00Is there a way to tell which micro is running softare so that software can adjust for the differences between upsd32xx and upsd33xx ie in the I2C code