Posted on January 13, 2009 at 04:56Hello, don't you forget to connect GND wire between your device and pin5 in the RS232 connecor? What does it mean -5V voltage on your schematics? Max232 needs only +5V to pin16 and GND to pin15
Posted on February 21, 2006 at 11:03Neila, thank you for yor reply! I know about DPP0...DPP3 registers, but it is not clear for me, how to use them together with MAC registers. There is another way to get access to any memory location: extp R12,#1 ...
Posted on February 17, 2006 at 05:12Hello! According to manual on ST10F269 MAC unit, command coMOV can be used for data transfer to the entire memory space: ''The GPR pointer allows access to the entire memory space, but IDXi are limited to the inte...
Posted on June 21, 2005 at 15:29At now I'm using ver 2.3C, is there is a plan to make update? If so, it is quite desirable to have possibility to use it in the command-line mode, because usually in the development process the filename is the same fo...
Posted on June 21, 2005 at 15:10Thank you for your reply ! The problem is solved: I simply changed linker settings and that's all. I don't use external ROM, so, as I understand, bit ROMS1 is primarily intended for switching between ext/int memory. I...