Posted on May 17, 2011 at 12:05I found the solution: In the document http://www.st.com/stonline/books/pdf/docs/7889.pdf there is an error in the schematic: At parallelport connector J1, pin 13 has to be connected with pin 8 and not with pin 20. I fo...
Posted on May 17, 2011 at 12:05Hello, I have built the Flashlink JTAG-Programmer according to this schematic: http://www.st.com/stonline/books/ascii/docs/7889.htm Unfortunately I always get an error message when trying to program a PSD834F2 via JTAG...
Posted on October 02, 2007 at 08:53Are the flash programming routines located in the XRAM2 address range (starting at 0xF0000) by the linker? If not, it only works, if your code is relocatable. If you have big loops for example, there are absolute j...
Posted on December 20, 2006 at 07:55Do you have a Pullup on P4.5 (CAN1_RXD)? ST10F276 does also have a built-in CAN-BSL. If there is a falling edge detected, CAN-BSL is started instead of UART-BSL.