Posted on May 09, 2005 at 07:36You need to first measure the fAWURC. The measurement mode can be eanbled by setting the AWUM bit. As you measure the frequency of any signal using Input Capture similarly you measure this frequency. Then as you have t...
Posted on May 09, 2005 at 06:45Regarding your fisrt problem - the watchdog problem please can you specify which Lite device you are referring to. Thanks to also elaborate on the problem because there is no known Wtachdog problem on any Lite MCU. Reg...
Posted on October 05, 2004 at 09:20Also refer section 4 for the cautions. ''Caution: During normal operation the ICCCLK pin must be pulled- up, internally or externally (external pull-up of 10k mandatory in noisy environment). This is to avoid enter...
Posted on October 05, 2004 at 09:20Also refer section 4 for the cautions. ''Caution: During normal operation the ICCCLK pin must be pulled- up, internally or externally (external pull-up of 10k mandatory in noisy environment). This is to avoid enter...
Posted on October 05, 2004 at 03:48Which MCU are you using? When using the LVD it is mandatory that you do not connect the pull-up resistance at the reset pin. Also please follow all the recommendations in the datasheet of the MCU which you are usin...