Posted on May 17, 2011 at 11:551. I know it is posible to disable each ''reset'' type seperatly. 2. The question is: AFTER I enable LVR and WD resets, WHEN I have a reset event, how can i find out which source was it. 3. Each reset deserve different...
Posted on May 17, 2011 at 11:55Thank you for the fast replay. Yes, i tried to make some experimnets with the DK-3200 kit. 1) I cancel the Watch Dog closing sequence, and the Watch Dog is functional there. 2) with my board the same experiment coused ...
Posted on May 17, 2011 at 11:55 Thank you for your fast reply. I don't think the problem caused by the Watch Dog because the first lines of code is kill the WD and all Interrupt sources. The code itself is at the end of my reply. The Hard...
Posted on May 17, 2011 at 11:551) The upsd run prgrams like port toggeling for 1 to 4 seconds then stop the prog and get lost. 2) The worm reset isn't work at all. only the POR reset work (mostly). the program includes zeroing the IE. why??????