Posted on March 17, 2005 at 10:24Hello, You assume that in the STPCKIT V2.1 you have changed the HWI2C_BASE_LSB parmater to HWI2C_BASE_LSB ||0x03 when writing in the Host configuration register 0x12 ? We will check this point and return to you to ...
Posted on March 08, 2005 at 04:23Hi, Which network adapter are you using ? Which network configuration are you using? Which is the version of CE that you use ? Tanks.
Posted on March 08, 2005 at 04:16Hi, Can you precise which STPC product are you using ? Could you please provide us the build.log file generated by the platform Builder in order to undestand the problem. Thanks.
Posted on January 17, 2005 at 11:42While the same build works fine on another board, the problem comes from the configuration of your PC104. I can suggest to you that you try the WinCE4.2, if the problem persists we are sure thet the problem is rela...