Posted on July 30, 2003 at 11:27We use the St10f269. We like to connect on TX(P3.0) an RX(P3.1) a PC with a Terminal Program so we can use the second port for diagnostic messages.
Posted on July 30, 2003 at 10:18We want to use port pin 3.0 and 3.1 for a second serial port, how can we configure that. it is clear that we have to change the value of the first three lines in the example for the first port. First Port: P3.10 and 3...
Posted on July 01, 2003 at 06:54 Thanks a lot for your help Max. i got the solution [ Diese Nachricht wurde editiert von : steff76 on 01-07-2003 10:25 ]
Posted on June 26, 2003 at 07:40It is not clear for me, for example we want to use p2.12 for waking up the ST10. Do we have to configure the p2.12 as a normal interrupt (CC12IO) and additonaly set the EXICON register??