Posted on April 10, 2003 at 14:14I would like to map an 8MByte FLASH ROM to the STPC ISA interface For my privious purpose of STPC Linux boot loader from FLASH It is mention in the user manual that when using FLASH that are bigger than 2Mbyte an add...
Posted on February 24, 2003 at 12:24 Thank you for your last answer We are building an ISA card for the flash. However I could not build my own kernel using the kernel script My kernel works fine using ''Linux kernel loader'' (loadlin, Li...
Posted on February 17, 2003 at 13:46Hi, Thank you your answer you recommand to use MTD in order to store a complete linux file system in flash I found another idea that was implemented on single board computer: Their conecpt is 1)load linux kernel u...