User Activity

HiFor the past few days I've been trying to get a dual core project with FreeRTOS and the LoRaWAN Stack for a custom STM32WL55 design to work but the CubeIDE seems to not properly generate everything that's required for it to work.When blindly genera...
HiI'm designing a custom PCB with a STM32MP157F and a DP83867 PHY connected over MDIO and RGMII. The problem is, the communication between the two is completely dead. No data or clock can be measured on either the MDIO or MDC line, MDIO is constant ...
Posted on May 09, 2018 at 20:29Hi.Is there a correct way of automatically detecting when my STM32 device gets connected to the computer through USB? I'm using .NET C♯ for my desktop application. For now I have to connect my device and then manually ...
Posted on May 22, 2017 at 21:01I'm working with the latest update of the HAL drivers for the STM32F446RET6. I want to use the RTC in my project and display the time on a display. The first call of HAL_RTC_GetTime works flawless and returns the curre...
Posted on November 27, 2016 at 17:10HiI try to send data over a VCP USB interface from my STM32F446RE to the computer. I use a C♯ programm with a SerialPort interface to read the data.Under Windows 7, 8 and 8.1 everything works perfectly fine but on...
Kudos from