User Activity

It should be possible?!I would like to capture a waveform coming in at PA8 (TIM1_CH1) and copy it to the output on PA9 (TIM1_CH2). The signal shortest time is about 8us.The waveform only needs to be copied from PA8 to PA9.All smart people would say, ...
This post can be removed as I found out what was wrong...But otherwise when you want to do DDR tuning some experienced quirks:- RTFM twice!- Make sure the target board is in Engineering Boot Mode!!- Notices that latest CubeMX and STM32CubeProgrammer ...
Is there a way to build only optee, etc. up to the level of u-boot?It would help to ease board bringup, checking the dts effects, do some basic testing. Regards,Roland 
I have a small micro that needs to run before the MP157 is active. The voltage coming gin is 5V, but I need 3.3V. Is there an always-on LDO in the STPMIC1 for such purpose? I assume the internal LDO is not te be used?Do I need to program the voltage ...
I have the latest FP-AI-VISION-1, the 747i-DISCO and the BCAM board. I can see the image, but cannot storen anything to a SDCARD. I tried an SDCard that is readable in the original 747i-DISCO demo code, so at least the interface and card seem to work...
Kudos from