User Activity

Hello,We are designing automotive devices (Trackets,Meters etc) and almost in all of our devices we use external watchdog with integrated BOD function.We faced issues in the past during EMC/ESD tests, where the microcontroller's (AVR) BOD or watchdog...
Hello,We have a device using the STM32F103 mC, driving an 320x480 display for basic shapes etc. We used SPI and then we moved to FSMC to increase speed.Now since STM32F103 is not dedicated for much applications and need more speed/better graphics, we...
Hello,We made a custom board based on STM32F746NG to drive a 5' TFT, using the TouchGFX library.Next step is to import a CANopen protocol stack (bought from 3rd party company) for Lift application. In general stack is running using one timer.Since To...
Hello,Does anyone managed to connect GT911 Touch Controller on STM32F746 Discovery or similar board; The demo project for STM32F746  [with TouchGFX] is using the FT5536.
Hello,We design a new custom PCB based on STM32F746G-DISCO board to support TouchGFX functionalities. Since the N25Q128A13EF840E Flash memory is obsolete, we are thinking about MT25QL128ABA1EW9-0SIT (same package - same pinout).The problem is that MT...
Kudos from