2018-02-11 11:04 AM
About two years ago, I did a comparison of C compilers for the STM8. It can now be found at
http://www.colecovision.eu/stm8/compilers-2016.shtml
.I also redid the comparison and placed it at
http://www.colecovision.eu/stm8/compilers.shtml
.For Cosmic, SDCC, IAR the current versions of the compilers were used. Due to difficulties with Raisonance evaluation licenses, an older version of Raisonance was used.
Quick summary of what happened since 2016: Cosmic and IAR improved a bit in various aspects. SDCC made huge progress. In mid-2016, code speed and size were weaknesses of SDCC. Now, for Dhrystone and Coremark, SDCC generates faster code than any other compiler (but floating-point performance and thus Whetstone scores are still bad). In terms of code size, it is now about on par with Cosmic, which means better than IAR and worse than Raisonance.
Philipp
#cosmic #sdcc #compiler #stm8 #iar2018-02-13 09:39 PM
Hello Philipp,
I tried one of the latest compiler builds. In my opinion, the quality of the generated code has improved noticeably. The problems what I discovered earlier are no longer valid.
2018-02-26 11:13 AM
The comparison has been updated by using a current version of Raisonance. However, except for tiny changes in Coremark scores and code size nothing changed.
Philipp
2018-04-21 12:34 AM
sdcc3.6.9 and 3.7.1 cannot compile uip stack. 'No more memory' if I remember correctly.
UIP stack is well known for being basically a very big C function.
My PC has 16G of RAM.
I was able to compile uip with sdcc3.6.0 though!
sdcc 3.6.0 generated 14K/16K binary where Cosmic generated 9K/10K. (two different programs, using uip stack).
Also, it compiles the uip stack in a veeeeery long time....