2022-09-21 6:06 AM
I'm using IAR 1.42.3
And I'm using Discovery kit with STM8S003K3 MCU.
I try to use the debug of Discovery kit in IAR but don't work.
When i use the ST Visual Develop using cosmic the debug works so good.
2022-09-21 6:40 AM
Welcome, @Jackson, to the community!
STM8S003K3 is included in the list of supported STM8 for the current version of IAR. If you do not have an outdated or limited version of IAR, you should contact IAR.
Does that answer your question for the time being?
Regards
/Peter
2022-09-21 6:42 AM
I see you are using IAR 1.42.3, the current version is 3.11. You probably need to upgrade to the new version.
2022-09-21 10:09 AM
Hi @Peter BENSCH thank you for answer my question. :)
I will to upgrade to the new version.
2022-12-16 6:10 AM
Have you upgraded it? I am waiting for your reply and till then I will visit https://letsgradeit.com/question/best-compare-and-contrast-essay-topics/ here because I want to know what are the best compare and contrast essay topics regarding my school project and after reading it, I will come back over here again and I hope someone replied my question answer.