cancel
Showing results for 
Search instead for 
Did you mean: 

UART2 Interrupt

uthenb
Associate II
Posted on June 24, 2010 at 10:36

Hello i'm port uart2 polling receive data from hyperterminal it's ok. but i need use uart2 receive data with interrupt?

  TIM3_DeInit();

 

  TIM3_TimeBaseInit(TIM3_PRESCALER_1,0xFFFF);

   TIM3_ITConfig(TIM3_IT_UPDATE, ENABLE);

    enableInterrupts();

    GPIO_Init(GPIOD, 0x01 , GPIO_MODE_OUT_PP_LOW_FAST);

       

    CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);

    UART2_DeInit();

    UART2_Init((u32)9600, UART2_WORDLENGTH_8D,    UART2_STOPBITS_1, UART2_PARITY_NO, UART2_SYNCMODE_CLOCK_DISABLE, UART2_MODE_TXRX_ENABLE);

    UART2_ClearITPendingBit(UART2_IT_RXNE);

    UART2_ITConfig(UART2_IT_IDLE, ENABLE);

this code incorrect i don't know use function and see a register please help me

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
saranyim
Associate II
Posted on March 14, 2011 at 09:43

TIM3_DeInit();

TIM3_TimeBaseInit(TIM3_PRESCALER_1,0xFFFF);

TIM3_ITConfig(TIM3_IT_UPDATE, ENABLE);

enableInterrupts();

GPIO_Init(GPIOD, 0x01 , GPIO_MODE_OUT_PP_LOW_FAST);

CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);

UART2_DeInit();

UART2_Init((u32)9600, UART2_WORDLENGTH_8D,    UART2_STOPBITS_1, UART2_PARITY_NO, UART2_SYNCMODE_CLOCK_DISABLE, UART2_MODE_TXRX_ENABLE);

UART2_ClearITPendingBit(UART2_IT_RXNE);

UART2_ITConfig(UART2_IT_IDLE, ENABLE);

UART2_ITConfig(UART2_IT_RXNE_OR, ENABLE);

fabioaymoto9
Associate II
Posted on May 11, 2011 at 13:47

I´m in doubt if I need to use the UART2_ClearITPendingBit() function after read a byte from UART2 Interruption routine, or the own read action clears the pending bit RXNE. I couldn´t find this information from RM0016 reference manual.

The code I´m using:

#ifdef _COSMIC_

@far @interrupt void UART2_RX_IRQHandler(void)

#else /* _RAISONANCE_ */

void UART2_RX_IRQHandler(void) interrupt 21

#endif /* _COSMIC_ */

{

  // Read one byte from the receive data register

  RxBuffer[RxCounter++] = UART2_ReceiveData8();

 

UART2_ClearITPendingBit(UART2_IT_RXNE_OR); // Does this function is necessary?

  

  if(

RxCounter==128)

    

   RxCounter=0;

  .

  .

  .

}

fabioaymoto9
Associate II
Posted on May 11, 2011 at 17:45

I´ve already tested here,  that function is not necessary.