2009-11-11 9:15 PM
TIM2 FWLIB Example
2011-05-17 6:05 AM
Hi,
Frupi, The HSI is selected as default clock source;) Regarding the CLK block diagram: the fHSI is divided by the prescaler that can be configured through HSIDIV[1:0] bits in the CLK_CKDIVR register (the reset value for these bit is 1 so, it divide the fHSI/4 by default) for more details refer to reference manual. When you use the mode output compare PWM1 you don't need to configure the interrupt. Coluber, Yes, the timerx(x=1,2,3,4,5) when available on the product (refer to product datasheet) is the same as the described one in the STM8S microcontroller family reference manual. Regards mozra