cancel
Showing results for 
Search instead for 
Did you mean: 

stvp issue on win 10 when programing stm8

andrei17
Associate

hello , 

i have an issue regarding stvp . before i used stvp on windows 7 and everything was working fine , but now i made an upgrade on windows 10 and it stops working. the error is ,,Cannot comunicate with the device .Check the swim cable .....'' If i try to program option bytes and verify them , it doesn t work , so in order to work i have to do it separately , and work only from second attempt. i have instaled the latest driver from st ,STSW-LINK009 and st_toolset pack 42 . 

what can i do to make it work like on windows 7?

 

2 REPLIES 2
Billy OWEN
ST Employee

Hi @andrei17 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

DarekR
Associate III
ST has practically stopped supporting STM8, which is incomprehensible to me, because it's their project, not a license. You can get around the incompatibility problem by using Windows 7 on Virtualbox. But ST should solve the problem. STM8s are great mkkrocontrollers for simple tasks.