cancel
Showing results for 
Search instead for 
Did you mean: 

STVD 4.1.4 bug (.NOLIST in ASM include files)

fggnrc
Associate II
Posted on January 15, 2010 at 10:46

STVD 4.1.4 bug (.NOLIST in ASM include files)

1 REPLY 1
fggnrc
Associate II
Posted on May 17, 2011 at 15:07

Dear Sirs,

I found a bug in how the latest STVD release manages ASM include files.

The attached archieve contains a default project to which I added MyInc.inc

This file contains only a .NOLIST directive and a #define.

After the project is successfully built, the simulator (and also my R-Link tool) gives this warning:

-> warning: remove white-space characters at the end of the last line of the include file

If I execute the code, there is no way to single-step through the code...

If I do as the warning suggests, the project can't be built.

Regards

EtaPhi

PS: a workaround is obviously to delete .NOLIST directives...