cancel
Showing results for 
Search instead for 
Did you mean: 

Stop iwdg in halt mode on STM8L051F3

PRasm.3
Associate II

Hey

I have tried to use the option byte to stop the iwdg when i enter halt.

I can see that i manage to set the WDG_HALTin option byte 3.

But the watchdog still resets the MCU after i enter halt.

Please help me, cant i do it? If so then how do i read that from the documentation.

If i can what am i doing wrong?

I can reproduce the problem with this code:

void halt_test(void) {
    // switch to 16MHz (default is 2MHz)
    sfr_CLK.CKDIVR.byte = 0x00;
 
    // Setup LED
    sfr_PORTB.DDR.DDR2 = 1; // input(=0) or output(=1)
    sfr_PORTB.CR1.C12 = 1;  // input: 0=float, 1=pull-up; output: 0=open-drain, 1=push-pull
 
    // Disable LED
    sfr_PORTB.ODR.ODR2 = 1;
 
    for (uint32_t i = 0; i < 600000; i++) {
        NOP();
    }
 
    // unlock w/e access to EEPROM & option bytes
    sfr_FLASH.DUKR.byte = 0xAE;
    sfr_FLASH.DUKR.byte = 0x56;
 
    // wait until access granted
    while (!(sfr_FLASH.IAPSR.DUL))
        ;
 
    // Enable write to option bytes
    sfr_FLASH.CR2.OPT = 1;
 
    // Set IWDG_HALT bit
    sfr_OPT.OPT3.byte = 0b10;
 
    // wait until end of programming
    while (!(sfr_FLASH.IAPSR.EOP))
        ;
 
    // Disable write to option bytes
    sfr_FLASH.CR2.OPT = 0;
 
    // lock EEPROM again against accidental erase/write
    sfr_FLASH.IAPSR.DUL = 0;
 
    // start IDWG (must be the first value written to this register, see UM)
    sfr_IWDG.KR.byte = (uint8_t)0xCC;
 
    // unlock write access to prescaler and reload registers
    sfr_IWDG.KR.byte = (uint8_t)0x55;
 
    sfr_IWDG.PR.PR = 6;
 
    // set timeout period 0xff = 1724.63ms according to RM0031
    sfr_IWDG.RLR.byte = 0xff;
 
    // start IDWG
    sfr_IWDG.KR.byte = (uint8_t)0xCC;
 
    // Enable LED
    sfr_PORTB.ODR.ODR2 = 0;
 
    ENTER_HALT();
}

This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15

No worries, i just saw you listed as an employee i guessed you had access to the board.

Do you know how to get in contact with somebody at st that have access to the chip?

Unfortunately no, the only options are your local distributor or OnLine Support OLS where you can open a personal ticket.

However, the STM8 are already set to NRND (Not Recommended for New Design), so there are practically no resources left for this obsolete technology.

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AA1
Senior III

Are you sure the watchdog resets while in halt?

Maybe program doesn't stop in halt.

PRasm.3
Associate II

I think i found the problem, but im not entirely sure why.

For start watchdog i set the KR register to CC in the code example. If i set it to AA instead everything seems to work as expected.

Would anybody know why that change would matter? I guess by reading the datasheet AA makes more sense but its not clear to me

Maybe value AA doesn't start watchdog. So reset doesn't occur.

From datasheet value AA starts watchdog, value CC refreshes watchdog.

Correction:

Maybe value AA doesn't start watchdog. So reset doesn't occur.

From datasheet value CC starts watchdog, value AA refreshes watchdog.