cancel
Showing results for 
Search instead for 
Did you mean: 

STM8S105 Interrupt Execution Time (using Raisonance Ride 7)

shtoh
Associate
Posted on October 28, 2010 at 10:34

STM8S105 Interrupt Execution Time (using Raisonance Ride 7)

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
lowpowermcu
Associate II
Posted on May 17, 2011 at 15:11

Hi toh.seng_huat,

why you don't use TIM1 in PWM mode ?

You can run timer counter in 1ms (as example) and channel 1 in pwm: ARR = 3000 and CCR1 = 2000 and you will get your signal without caring about it in software. Your CPU will be loaded-off.

MCU Lüfetr

shtoh
Associate
Posted on May 17, 2011 at 15:11

Hi lowpowermcu,

Actually, i'm testing on a pre-designed pcb circuit, so my timer 1 does not connect to any LEDs, only timer3 does. That's why i'm using timer3.

Understands that setting CCR to the ratio of the ARR can get the desired outcome... As i need to show that I can use PWM mode to make the LED glow and off.

Currently I manage to get the effect on and going.

Thanks a lot.

Hi toh.seng_huat,

why you don't use TIM1 in PWM mode ?

You can run timer counter in 1ms (as example) and channel 1 in pwm: ARR = 3000 and CCR1 = 2000 and you will get your signal without caring about it in software. Your CPU will be loaded-off.

MCU Lüfetr