cancel
Showing results for 
Search instead for 
Did you mean: 

Stm8s Discovery project with stts75 sensor and µoled display

RomainR.
ST Employee
Posted on November 30, 2010 at 10:31

hello all

Please find attached file source code and resources on my recent personal project.

Stm8s-Discovery is interfaced with astts75 chip (digital I²C temprature sensor) and a graphic serialdisplay of the manufacturer μOled 96-SG1 4DSystems.

The accuracy of the temperature sensor can beselected by softwarefrom 0.5 ° C, 0.25 ° C, 0125 ° Cto 0.0625 ° C.

The scale measuring ranges from -55 ° C to +125 ° C.

The main program just displays the temperature on μOled with 0.5°C of accuracy.

I hope to improve this project very soon.

You can find the datasheet of stts75 here:

http://www.st.com/internet/analog/product/169jsp

4DSystems μOled display and serial here:

http://www.4dsystems.com.au/prod.php?id=77

Regards

Romain.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
brazov22
Associate II
Posted on December 01, 2010 at 15:12