cancel
Showing results for 
Search instead for 
Did you mean: 

STM8L SD Card

ahmad sina
Associate II
Posted on January 18, 2017 at 17:31

i need your help about drive micro SD card with STM8L101F3P6

i use the library of Eval-Board of STM8l151 for this

and i have no error in compile Code but the stm failed in initalize routine of SD and can not init this.

So the MCU cant write data on SD Card

what Capacity of SD i can use.

#stm #stm8l101xx #stm8l151c6t6 #sd-card
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on January 18, 2017 at 18:25

Without looking at the code I'd assume it is fit for SD cards of 2GB and below, and will not support SDHC or SDXC cards which use a slightly different command structure.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on January 19, 2017 at 11:25

hello

thanks for your attention

so i test this and send you the the answer

On Wed, Jan 18, 2017 at 8:56 PM, Clive One <st-microelectronics@jiveon.com>

Posted on January 19, 2017 at 12:02

hello

i test this option and use the SD card not SDHC or SDXC with 2G Capacity

but still not work