2026-01-21 7:05 AM
Hi,
I have few custom boards with STM32MP257 mostly running PTP related tasks. Once in a while (once in a few days of continuous run) I have noticed the following error in the dmesg (as it seems UART related - I have 4 UARTs enabled in the DT, while 3 of them have DMA enabled (the console one does not have the DMA enabled), but only one UART (other than console) is being used in the system for RX only):
[251158.390476] Unable to handle kernel paging request at virtual address dead000000000108
[251158.392934] Mem abort info:
[251158.395854] ESR = 0x0000000096000044
[251158.399679] EC = 0x25: DABT (current EL), IL = 32 bits
[251158.405114] SET = 0, FnV = 0
[251158.408235] EA = 0, S1PTW = 0
[251158.411457] FSC = 0x04: level 0 translation fault
[251158.416489] Data abort info:
[251158.419408] ISV = 0, ISS = 0x00000044, ISS2 = 0x00000000
[251158.425041] CM = 0, WnR = 1, TnD = 0, TagAccess = 0
[251158.430173] GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[251158.435607] [dead000000000108] address between user and kernel address ranges
[251158.442949] Internal error: Oops: 0000000096000044 [#1] PREEMPT SMP
[251158.449289] Modules linked in: marvell cfg80211 rfkill usb_f_ncm u_ether libcomposite spidev crct10dif_ce phy_stm32_usb2phy rtc_stm32 mr75203 hantro_vpu v4l2_jpeg v4l2_vp9 v4l2_h264 v4l2_mem2mem videobuf2_dma_contig videobuf2_memops videobuf2_v4l2 videodev at24 videobuf2_common mc stm32_cryp dwc3_stm32 stm32_lptimer crypto_engine spi_stm32 libdes stm32_crc32 stm32_timers mailbox_client_cdev stm32_m0_rproc stm32_rproc irq_rpmsg sch_fq_codel nfnetlink ip_tables ipv6
[251158.490832] CPU: 0 PID: 243312 Comm: kworker/0:2 Not tainted 6.6.78-gaf978724e078-dirty #1
[251158.499183] Hardware name: STMicroelectronics STM32MP257F CARD (DT)
[251158.505923] Workqueue: pm pm_runtime_work
[251158.510064] pstate: 200000c5 (nzCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[251158.517110] pc : vchan_tx_submit+0x58/0xd0
[251158.521343] lr : vchan_tx_submit+0x28/0xd0
[251158.525574] sp : ffff8000828cbba0
[251158.528997] x29: ffff8000828cbba0 x28: 0000000000000000 x27: 0000000000000000
[251158.536250] x26: ffff0000040fdcf4 x25: 0000000000000000 x24: 0000000000000000
[251158.543502] x23: 0000000000000000 x22: ffff000006d5c780 x21: ffff00000494a6a0
[251158.550754] x20: 000000000003d505 x19: ffff0000064823c0 x18: 0000000000000000
[251158.558006] x17: ffff7fffb5e89000 x16: ffff800080000000 x15: 001015373f0be4e6
[251158.565259] x14: 0000000000000001 x13: 0000000000000001 x12: 0000000000000001
[251158.572510] x11: 0000000000000000 x10: 0000000000000003 x9 : 0000000000000000
[251158.579762] x8 : ffff00000494a748 x7 : 0000000000084000 x6 : 0000000000000800
[251158.587014] x5 : ffff00000494a758 x4 : dead000000000100 x3 : dead000000000122
[251158.594266] x2 : ffff000006482438 x1 : 0000000000000000 x0 : ffff00000494a740
[251158.601518] Call trace:
[251158.604038] vchan_tx_submit+0x58/0xd0
[251158.607968] stm32_usart_rx_dma_start_or_resume+0xd8/0x234
[251158.613509] stm32_usart_runtime_resume+0x78/0xe8
[251158.618344] pm_generic_runtime_resume+0x2c/0x44
[251158.623081] __genpd_runtime_resume+0x30/0x80
[251158.627517] genpd_runtime_resume+0x114/0x29c
[251158.631954] __rpm_callback+0x48/0x1d8
[251158.635788] rpm_callback+0x6c/0x78
[251158.639420] rpm_resume+0x490/0x6b4
[251158.642952] pm_runtime_work+0x84/0xc8
[251158.646882] process_one_work+0x144/0x29c
[251158.650917] worker_thread+0x324/0x43c
[251158.654848] kthread+0x110/0x114
[251158.658077] ret_from_fork+0x10/0x20
[251158.661813] Code: 1a9fc694 b9001074 b8078454 a9478e64 (f9000483)
[251158.668051] ---[ end trace 0000000000000000 ]---
[251158.672781] note: kworker/0:2[243312] exited with irqs disabled
[251158.679385] note: kworker/0:2[243312] exited with preempt_count 1
after this event, the system begins acting strangely - the heartbeat led blinking much faster than usual (although top command does not seem to show high CPU load, some services cannot be stopped - like I can run journalctl of some process, but I cannot stop it, the process just getting hang and kill does not help.
Any ideas of what can cause it?
Thanks!
Alexey.
Solved! Go to Solution.
2026-04-15 7:16 AM
Hello @altsir_sga , @MGO75 ,
Could you please try to apply the enclosed patch on your Linux kernel, and see if you still face troubles ?
We observed a use after free in the suspend / resume sequence due to a missing lock mechanism. This patch should solve the situation.
Kind regards,
Erwan.
2026-01-21 8:32 AM
After further investigating the issue, from the call trace it seems to be related to waking up from suspension. My UART receives NMEA data once in the second so I guess the UART goes to sleep between the NMEA packets and this happens once in a second.
May be it will help....
Alexey.
2026-02-03 7:10 AM
Hi,
We are facing a similar issue with USART1 (UART) connected to a Bluetooth chip on an STM32MP255 device. In many cases, after a suspend/resume cycle the system hits a kernel crash/oops, and the UART stops working afterwards (the Bluetooth interface is no longer functional):
[ 822.398942] Unable to handle kernel paging request at virtual address dead000000000108
[ 822.401306] Mem abort info:
[ 822.404026] ESR = 0x0000000096000044
[ 822.407750] EC = 0x25: DABT (current EL), IL = 32 bits
[ 822.413085] SET = 0, FnV = 0
[ 822.416107] EA = 0, S1PTW = 0
[ 822.419228] FSC = 0x04: level 0 translation fault
[ 822.424059] Data abort info:
[ 822.426878] ISV = 0, ISS = 0x00000044, ISS2 = 0x00000000
[ 822.432311] CM = 0, WnR = 1, TnD = 0, TagAccess = 0
[ 822.437343] GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[ 822.442676] [dead000000000108] address between user and kernel address ranges
[ 822.449718] Internal error: Oops: 0000000096000044 [#1] PREEMPT SMP
[ 822.455957] Modules linked in: hci_uart btbcm brcmfmac_cyw brcmfmac brcmutil galcore(O) stm32_dcmipp stm32_lptimer stm32_csi stm32_cryp crypto_engine stm32_crc32 spi_stm32 optee_rng nfnetlink
[ 822.472908] CPU: 0 PID: 89 Comm: kworker/0:7 Tainted: G W O 6.6.78-dey-37241-g4adaf6e6e4e4 #1
[ 822.490211] Workqueue: pm pm_runtime_work
[ 822.494154] pstate: 200000c5 (nzCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 822.501099] pc : vchan_tx_submit+0x58/0x8c
[ 822.505137] lr : vchan_tx_submit+0x28/0x8c
[ 822.509272] sp : ffff800081e9bba0
[ 822.512494] x29: ffff800081e9bba0 x28: 0000000000000000 x27: 0000000000000000
[ 822.519646] x26: ffff000005d6ecf4 x25: 0000000000000000 x24: 0000000000000000
[ 822.526698] x23: 0000000000000000 x22: ffff000006b4a120 x21: ffff0000064d26a0
[ 822.533850] x20: 00000000000000db x19: ffff00000948d240 x18: 0000000000000000
[ 822.540901] x17: 0000000000000000 x16: 0000000000000000 x15: 000022af3f21217e
[ 822.548052] x14: ffff000005ee6810 x13: 0000000000000000 x12: 0000000000000001
[ 822.555104] x11: 0000000000000000 x10: 0000000000000001 x9 : 0000000000000002
[ 822.562255] x8 : ffff0000064d2748 x7 : 0000000000084000 x6 : 0000000000000800
[ 822.569307] x5 : ffff0000064d2758 x4 : dead000000000100 x3 : dead000000000122
[ 822.576459] x2 : ffff00000948d2b8 x1 : 0000000000000000 x0 : ffff0000064d2740
[ 822.583512] Call trace:
[ 822.585931] vchan_tx_submit+0x58/0x8c
[ 822.589664] stm32_usart_rx_dma_start_or_resume+0xd8/0x234
[ 822.595108] stm32_usart_runtime_resume+0x78/0xe8
[ 822.599746] pm_generic_runtime_resume+0x2c/0x44
[ 822.604381] __genpd_runtime_resume+0x30/0x80
[ 822.608715] genpd_runtime_resume+0x110/0x244
[ 822.613049] __rpm_callback+0x48/0x1d8
[ 822.616781] rpm_callback+0x6c/0x78
[ 822.620211] rpm_resume+0x490/0x6b4
[ 822.623641] pm_runtime_work+0x84/0xc8
[ 822.627372] process_one_work+0x144/0x29c
[ 822.631409] worker_thread+0x31c/0x434
[ 822.635142] kthread+0x110/0x114
[ 822.638272] ret_from_fork+0x10/0x20
[ 822.641809] Code: 1a9fc694 b9001074 b8078454 a9478e64 (f9000483)
[ 822.647947] ---[ end trace 0000000000000000 ]---We observed that reverting ST’s commit https://github.com/STMicroelectronics/linux/commit/83771e186d2abeccc38b0a5e6841b068499622ca improves the behavior (the issue becomes less frequent / the system is more stable), but the problem is not fully resolved and we still hit the same failure after suspend/resume.
Any help would be appreciated,
Arturo.
2026-02-03 8:29 AM
Hi,
I have ended up disabling the suspend mode for all UARTS (as my device is always powered, I don't need it):
Didn't have any issues since then.
Alexey.
2026-03-31 4:53 AM
We have the same problem by using UART5 on STM32MP233 and STM32MP257. After a couple of minutes, sometimes hours, the driver stm32-usart crashed (Oops kernel panic). But it only occurs when using DMA at this uart, if we delete the DMA properties, it runs fine. Thanks to @altsir_sga for commit the patch of the usart driver. Disabling the suspend mode for all uarts is a better choice, i think. So we can use DMA again and it works now without problems.
With best reagrds Maik
[ 6720.887991] Unable to handle kernel paging request at virtual address dead000000000108
[ 6720.890352] Mem abort info:
[ 6720.893072] ESR = 0x0000000096000044
[ 6720.896897] EC = 0x25: DABT (current EL), IL = 32 bits
[ 6720.902131] SET = 0, FnV = 0
[ 6720.905153] EA = 0, S1PTW = 0
[ 6720.908276] FSC = 0x04: level 0 translation fault
[ 6720.913207] Data abort info:
[ 6720.916026] ISV = 0, ISS = 0x00000044, ISS2 = 0x00000000
[ 6720.921560] CM = 0, WnR = 1, TnD = 0, TagAccess = 0
[ 6720.926592] GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[ 6720.931826] [dead000000000108] address between user and kernel address ranges
[ 6720.938969] Internal error: Oops: 0000000096000044 [#1] PREEMPT SMP
[ 6720.945210] Modules linked in: 8021q garp mrp sch_prio sch_mqprio sch_mqprio_lib ksz8863_smi ksz_switch dsa_core bridge stp llc edgx_pfm_lkm(O) stm32_deip(O)
[ 6720.959345] CPU: 0 PID: 479 Comm: kworker/0:0 Tainted: G O 6.6.78-gf01241fbba4d-dirty #1
[ 6720.968802] Hardware name: STMicroelectronics custom STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06 (DT)
[ 6720.979863] Workqueue: pm pm_runtime_work
[ 6720.983908] pstate: 200000c5 (nzCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 6720.990854] pc : vchan_tx_submit+0x58/0xd0
[ 6720.994887] lr : vchan_tx_submit+0x28/0xd0
[ 6720.999018] sp : ffff80008452bba0
[ 6721.002341] x29: ffff80008452bba0 x28: 0000000000000000 x27: 0000000000000000
[ 6721.009394] x26: ffff0000041afcf4 x25: 0000000000000000 x24: 0000000000000000
[ 6721.016547] x23: 0000000000000000 x22: ffff000008cbf960 x21: ffff000004972080
[ 6721.023700] x20: 0000000000000183 x19: ffff000004030840 x18: 0000000000000001
[ 6721.030853] x17: 0000000000000000 x16: 0000000000000000 x15: 000aa41b009aa29e
[ 6721.037905] x14: 0000000000000001 x13: 0000000000000001 x12: 0000000000000001
[ 6721.045058] x11: 0000000000000000 x10: 0000000000000003 x9 : 0000000000000000
[ 6721.052211] x8 : ffff000004972128 x7 : 0000000000084000 x6 : 0000000000000800
[ 6721.059263] x5 : ffff000004972138 x4 : dead000000000100 x3 : dead000000000122
[ 6721.066416] x2 : ffff0000040308b8 x1 : 0000000000000000 x0 : ffff000004972120
[ 6721.073570] Call trace:
[ 6721.075989] vchan_tx_submit+0x58/0xd0
[ 6721.079720] stm32_usart_rx_dma_start_or_resume+0xd8/0x234
[ 6721.085162] stm32_usart_runtime_resume+0x78/0xe8
[ 6721.089899] pm_generic_runtime_resume+0x2c/0x44
[ 6721.094535] __genpd_runtime_resume+0x30/0x80
[ 6721.098869] genpd_runtime_resume+0x114/0x29c
[ 6721.103204] __rpm_callback+0x48/0x1d8
[ 6721.106936] rpm_callback+0x6c/0x78
[ 6721.110366] rpm_resume+0x490/0x6b4
[ 6721.113897] pm_runtime_work+0x84/0xc8
[ 6721.117629] process_one_work+0x144/0x29c
[ 6721.121561] worker_thread+0x31c/0x434
[ 6721.125291] kthread+0x110/0x114
[ 6721.128522] ret_from_fork+0x10/0x20
[ 6721.132158] Code: 1a9fc694 b9001074 b8078454 a9478e64 (f9000483)
[ 6721.138196] ---[ end trace 0000000000000000 ]---
[ 6721.142826] note: kworker/0:0[479] exited with irqs disabled
[ 6721.148745] note: kworker/0:0[479] exited with preempt_count 1
2026-04-10 2:23 AM
Hello @altsir_sga,
We found several bugs in UART driver related to auto-suspend : the fixes will be available in the next Ecosystem-v6.2.1 planned end of June.
BR,
Christophe
2026-04-15 7:16 AM
Hello @altsir_sga , @MGO75 ,
Could you please try to apply the enclosed patch on your Linux kernel, and see if you still face troubles ?
We observed a use after free in the suspend / resume sequence due to a missing lock mechanism. This patch should solve the situation.
Kind regards,
Erwan.
2026-04-15 7:50 AM
Hi Erwan,
Will give it a try and get back to you.
Regards,
Alexey.
2026-04-20 7:15 AM
Hi Erwan,
I have tested this version for a few days now and it seems that it resolves the issue as the crash didn't happen.
Thanks!
Alexey.
2026-04-20 7:47 AM
Hello @altsir_sga ,
That was nice of you to let us know. I am glad to see this situation solved on your side.
Kind regards,
Erwan.