cancel
Showing results for 
Search instead for 
Did you mean: 

stm8_uart1.c error

pok-on
Associate II
Posted on October 16, 2013 at 10:36

Hello,

I am not sure if this is a proper place for reporting errors. If not so, please tell me, where to report it.

The error is in stm8_uart1.c module of STM8S_StdPeriph_Lib_V2.1.0.

According to description of UART1_ITConfig one of the parameters can have value UART1_IT_RXNE or UART1_OR. When using one of these, the assert_failed function will be called as macro IS_UART1_CONFIG_IT_OK(UART1_IT) treat them as invalid parameters. Using parameter UART1_IT_RXNE_OR works well with the same effect, but at least the description of UART1_ITConfig should be corrected to safe developers time ;-).

#uart1_itconfig-stm8s_stdperiph
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Dmitry Key
Associate II
Posted on February 25, 2018 at 09:56

Same here. Had to replace function call with simple

UART1->CR2 |= (uint8_t)UART1_FLAG_RXNE;