cancel
Showing results for 
Search instead for 
Did you mean: 

STM8/128 demo fw broken (UARTs)

Philipp Krause
Senior III
Posted on December 21, 2013 at 16:23

The STM8/128-EVAL demo firmware provided by ST is broken:

It does not correctly enable the output pins for the TX lines. Thus you will never see anything on the USARTs in the adc demos that are supposed to use them.

Philipp

P.S.: I've put a simple, working USART demo for the STM8/128-EVAL at

http://www.colecovision.eu/stuff/stm8/

it repeatedly outputs ''Hello world!'' at 1200 baud, 1 stop bit.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Philipp Krause
Senior III
Posted on December 21, 2013 at 23:38

I replaced the demo by one for 9600 baud.

Philipp Krause
Senior III
Posted on October 26, 2014 at 17:22

Based on the demo I wrote a short tutorial on serial I/O using sdcc on the STM8/128-EVAL:

http://www.colecovision.eu/stm8/128-EVAL%20Serial.shtml

Philipp

zzdz2
Associate II
Posted on October 27, 2014 at 08:47

I noticed a little problem.

These html lines:

#include 

<stdint.h>

#include 

<stdio.h>

are shown as empty '#include' in the browser.

Philipp Krause
Senior III
Posted on October 27, 2014 at 09:59

Thanks. It is fixed now (in all three tutorials that were affected).

Philipp