cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-IHM029V1 firmware built problem.

enlai
Associate
Posted on October 07, 2013 at 16:36

Hi.

I recently receive the

STEVAL-IHM029V1

demo board, with the firmware code on a CD, I installed the STVD software and the COSMIC compiler I setup everything, but I can not get the firmware compiled, If there is somebody that could help me please.

the error I get on the STVD is:

Running Linker

clnk -m Debug\ihm029_v1.map -l''C:\Program Files\COSMIC\CXSTM8_32K\Lib''  -o Debug\ihm029_v1.sm8 Debug\ihm029_v1.lkf

&sharperror clnk Debug\ihm029_v1.lkf:1 no default placement for segment .Signature

 The command: ''clnk -m Debug\ihm029_v1.map -l''C:\Program Files\COSMIC\CXSTM8_32K\Lib''  -o Debug\ihm029_v1.sm8 Debug\ihm029_v1.lkf '' has failed, the returned value is: 1

exit code=1.

ihm029_v1.elf - 3 error(s), 0 warning(s)

I would appreciate any help.

Thanks in advance.

#steval-ihm029v1
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0