SPI Master Mode
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-10-04 12:10 AM
Posted on October 04, 2013 at 09:10
Hi,
I am facing problem in SPI master mode configuration. I can't see any response on MISO line (Slave is tested OK). Here is my SPI initialize functions. void SPI_init() { SPI->CR1 = SPI_CR1_RESET_VALUE; // Reset value SPI->CR2 = SPI_CR2_RESET_VALUE; SPI->ICR = SPI_ICR_RESET_VALUE; SPI->SR = SPI_SR_RESET_VALUE; SPI->DR = SPI_DR_RESET_VALUE; SPI->CRCPR = SPI_CRCPR_RESET_VALUE ; SPI->RXCRCR = SPI_RXCRCR_RESET_VALUE; SPI->TXCRCR = SPI_TXCRCR_RESET_VALUE; GPIOC->ODR = 0; // MISO - C7 GPIOC->DDR = 0x60; // SCK - C5 GPIOC->CR1 = 0x60; // MOSI - C6 GPIOC->CR2 = 0x60; // o/p with 10 MHz capacity SPI->CR1 = 0x3c; // MSB first-250K-master-pol=0-phase=0 SPI->CR2 = 0x03; // SSn is driven by s/w GPIOD->ODR |= 0x08; // SSn i/o pin=1 } void spi_transactor (unsigned char wlength, unsigned char rlenght, const unsigned char *write_data, unsigned char *read_data) { unsigned char transaction_length = wlength + rlenght; unsigned char i; unsigned char dummy; unsigned char temp; GPIOD->ODR &= 0xF7; // SSn = 0 SPI->CR1 |= SPI_CR1_SPE; // SPI enable for (i=0; i<transaction_length; i++) { while(((SPI->SR) & (SPI_SR_TXE)) != 0x02); // Wait until TXE Flag = 1 if(i >= wlength) SPI->DR = 0x00; else SPI->DR = *write_data++; while(((SPI->SR) & (SPI_SR_RXNE)) != 0x01); if(i >= wlength) *read_data++ = SPI->DR; else dummy = SPI->DR; } while(((SPI->SR) & SPI_SR_BSY) == 0x80); SPI->CR1 &= ~SPI_CR1_SPE; // SPI Disable GPIOD->ODR |= 0x08; // SSn=1 } Using these functions I am sending/receiving data to/from slave. I can see data on MOSI line but not on MISO. Any suggestions for ''spi_transactor'' definition ??? #spi-master-mode
Labels:
- Labels:
-
SPI
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0