cancel
Showing results for 
Search instead for 
Did you mean: 

Reliability of STM8S internal MVR...

VPant.1
Associate

Because I don't find related information elsewhere (datasheet, application notes, etc.) I would ask it there.

So, I have famous W1209 thermostat board with Nuvoton MCU, which I'm replace by an STM8S103F3.

For proper operation it is needed to place an capacitor between VCAP and GND pins​.

There is exactly place where trouble occurred: unluckily capacitor was been shorted, so, I'm literally shorts MVR to GND.

When I'm connected to MCU via ST-LINK (5

Volt, SWIM, RST and GND) MCU isn't respond, don't allowing any kind of data exchanging.

When I'm checking state of MCU by finger (old danger behavior, I know) I'm nearly burn it and immediately disable ST-LINK adapter.

When I replaced damaged capacitor by right one, MCU allows at least flash/register state reading.

So, question: did my STM8S is reliable now, after nearly minute-two short circuited their MVR to ground and powered by ST-LINK?

Or, it is better to replace them?

How to check MVR reliability?

Or, maybe, MVR had an OCP, so no worry at all?

With best regards, Vladyslav Pantilimonov.​

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0