cancel
Showing results for 
Search instead for 
Did you mean: 

Raisonance CodeCompressor through STVD 4.1.2

abogani9
Associate II
Posted on June 16, 2009 at 08:33

Raisonance CodeCompressor through STVD 4.1.2

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
abogani9
Associate II
Posted on May 17, 2011 at 15:03

Hi,

I have noticed that the just released STVD 4.1.2 support the Raisonance's codecompressor. I found this feature very useful so I go immediatly to test it.

Unfortunately it hang without end on my personal computer at:

[...]

LINK/LOCATE RUN COMPLETE, NO ERROR FOUND.

ccompst7_7.exe Debug\program.aof -O(Debug\program.aof) -AOF -NOHEX -C -T(2)

[...]

It is also eat the 50% of my AthlonX2 5600+ (2,9Ghz).

Could anyone point me at workaround?

Thanks!

Ciao,

Alessio

mozra27
Associate II
Posted on May 17, 2011 at 15:03

Hi Bogani,

The code compressor with STVD use the defined option: -AOF -NOHEX -C -T(2) if you have an issue with this configuration you can check an other specific option by running the command line:

The command line syntax is:

\Bin\ccompst7_7.exe aofname [options]

Where options may be:

-C complete process (in lining, factorizing, saving)

-I inlining process without any limitation

-IN(value) inlining process with number of in lined functions limited up to value

-F factorizing process without any limitation

-FN(value) factorizing process with a number of factorizations limited up to value

-FS(value) factorizing process with a minimum gain of value bytes per factorization

-FD(value) factorizing process with a maximum gain of value bytes per factorization

-LF log file generation

-T(variant) Define the processor variant: 0 for ST7 (default) and 2 for STM8.

-V(level) verbose level on level value

-[NO]AOF generate [not] an OMF-ST7 file (default is NOAOF)

-[NO]HEX generate [not] a HEX file (default is HEX)

-[NO]BIN generate [not] a BINARY file (default is NOBIN)

Regards

mozra