cancel
Showing results for 
Search instead for 
Did you mean: 

MCU STM8 as SPI slave

k.s.corp
Associate II

Hello. I want to make the controller a slave for the SPI. I understand the hardware activation Support leg stm8 at present, as it was then activated receiving \ transmitting?

/* Includes ------------------------------------------------------------------*/
#include "stm8s.h"
 
/* Private defines -----------------------------------------------------------*/
#define TIM4_PERIOD 124
#define USER_TIME_CYCLE 10
 
unsigned int system_plc_time = USER_TIME_CYCLE;
bool Start_SPI = FALSE;
//bool Start_SPI = TRUE;
uint8_t system_buff_mb_msg_rx[10];
 
/* Private function prototypes -----------------------------------------------*/
static void CLK_Config(void);
static void TIM4_Config(void);
static void SPI_Config(void);
static void EXTI_Config(void);
 
/* Private functions ---------------------------------------------------------*/
static void CLK_Config(void)
{
  CLK_DeInit();
  CLK_HSICmd(ENABLE);
  CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
  CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
  //CLK_CCOConfig(CLK_OUTPUT_MASTER);
}
 
static void TIM4_Config(void)
{
  TIM4_DeInit();
  TIM4_TimeBaseInit(TIM4_PRESCALER_128, TIM4_PERIOD);
  TIM4_ClearFlag(TIM4_FLAG_UPDATE);
  TIM4_ITConfig(TIM4_IT_UPDATE, ENABLE);
  TIM4_Cmd(ENABLE);
  TIM4_ClearITPendingBit(TIM4_IT_UPDATE);
}
 
static void SPI_Config(void)
{
  SPI_DeInit();
  SPI_Init(SPI_FIRSTBIT_MSB,
           SPI_BAUDRATEPRESCALER_2,
           SPI_MODE_SLAVE,
           SPI_CLOCKPOLARITY_LOW,
           SPI_CLOCKPHASE_1EDGE,
           SPI_DATADIRECTION_2LINES_FULLDUPLEX,
           SPI_NSS_SOFT,
           0x07);
  SPI_NSSInternalSoftwareCmd(DISABLE);
  SPI_ITConfig(SPI_IT_RXNE, ENABLE);
  //SPI_ITConfig(SPI_IT_WKUP, ENABLE);
  SPI_Cmd(ENABLE);
}
 
static void EXTI_Config(void)
{
  EXTI_DeInit();
  GPIO_Init(GPIOA, GPIO_PIN_3, GPIO_MODE_IN_PU_IT);
  EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOA, EXTI_SENSITIVITY_FALL_LOW);
  
}
 
INTERRUPT_HANDLER(TIM4_UPD_OVF_IRQHandler, 23)
{
   disableInterrupts();
   system_plc_time--;
   TIM4_ClearITPendingBit(TIM4_IT_UPDATE);
   enableInterrupts();
}
 
INTERRUPT_HANDLER(SPI_IRQHandler, 10)
{
  disableInterrupts();
  //if (Start_SPI == TRUE)
  //{
    Start_SPI = FALSE;
    //SPI_ITConfig(SPI_IT_RXNE, DISABLE);
    system_buff_mb_msg_rx[0] = SPI_ReceiveData();
    SPI_SendData(system_buff_mb_msg_rx[0]);
  //}
  enableInterrupts();
}
 
INTERRUPT_HANDLER(EXTI_PORTA_IRQHandler, 3)
{
  disableInterrupts();
  Start_SPI = TRUE;
  //SPI_ITConfig(SPI_IT_RXNE, ENABLE);
  enableInterrupts();
}
 
void main(void)
{
  CLK_Config();
  TIM4_Config();
  SPI_Config();
  EXTI_Config();
  enableInterrupts();
  
  /* Infinite loop */
  while (1)
  {    
    if(!system_plc_time)
    {
      //SPI_SendData(127);
      system_plc_time = USER_TIME_CYCLE;
    }
  }
  
}
 
 
#ifdef USE_FULL_ASSERT
 
/**
  * @brief  Reports the name of the source file and the source line number
  *   where the assert_param error has occurred.
  * @param file: pointer to the source file name
  * @param line: assert_param error line source number
  * @retval : None
  */
void assert_failed(u8* file, u32 line)
{ 
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 
  /* Infinite loop */
  while (1)
  {
  }
}
#endif

in code i rx/tx one byte for test

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0