is the i2c init function right?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-12-01 7:49 PM
void sEE_Init(void)
{
//printf("i2c init\n");
sEE_LowLevel_Init(); // enable clock
/*!< I2C configuration */
/* sEE_I2C Peripheral Enable */
I2C_Cmd(sEE_I2C, ENABLE);
I2C_DeInit(sEE_I2C);
/* sEE_I2C configuration after enabling it */
I2C_Init(sEE_I2C, I2C_SPEED, I2C_SLAVE_ADDRESS7, I2C_Mode_I2C, I2C_DutyCycle_2,
I2C_Ack_Enable, I2C_AcknowledgedAddress_7bit);
/* Enable the sEE_I2C peripheral DMA requests */
//I2C_DMACmd(sEE_I2C, ENABLE);
#if defined (sEE_M24C64_32)
/*!< Select the EEPROM address according to the state of E0, E1, E2 pins */
sEEAddress = sEE_HW_ADDRESS;
#endif /*!< sEE_M24C64_32 */
}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0