cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt not working

ST MICROCONTOLLER
Associate II
Posted on December 21, 2016 at 13:02

I am trying to run a code in which timer causes an interrupt and everytime interrupt is generated, a variable h is incremented, but it remains zero in quickwatch window. My code is written below in stvd and cosmic compiler.

#include 'stm8s.h'

#include 'stm8s_tim1.h'

#include 'stm8s_itc.h'

#define TIM1_PSCRH (*(volatile uint8_t *)0x5260)

#define TIM1_CR1    (*(volatile uint8_t *)0x5250)

#define TIM1_ARRH    (*(volatile uint8_t *)0x5263)

#define TIM1_ARRL    (*(volatile uint8_t *)0x5264)

#define TIM1_PSCRL    (*(volatile uint8_t *)0x5261)

#define TIM1_IER (*(volatile uint8_t *)0x5254)

int h;

void main(void)

{

            //TIM1_SetCounter(5);enableInterrupts();GPIO_Config();

            //TIM1_DeInit();

TIM1_ARRH=0X55;

TIM1_ARRL=0X26;

TIM1_PSCRH = 0x3e;

TIM1_PSCRL = 0x80;

TIM1_CR1=0X81;

TIM1_IER=0X01;

enableInterrupts();

      while(1)

      {

        

       }

         }

INTERRUPT_HANDLER (TIM1_UPD_OVF_IRQHANDLER,23)

//@interrupt @far void TIM1_OVF_TRG_BRK_IRQ_Handler(void)

{

    h++;

}

    

#ifdef USE_FULL_ASSERT

/**

  * @brief  Reports the name of the source file and the source line number

  *   where the assert_param error has occurred.

  * @param file: pointer to the source file name

  * @param line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t* file, uint32_t line)

{

  /* User can add his own implementation to report the file name and line number,

     ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */

  /* Infinite loop */

  while (1)

  {

  }

}

#endif

What is wrong with the code? Kindly help me.

Thank you.

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Posted on January 04, 2017 at 22:08

NVIC is the CortexM interrupt controller in STM32 devices. Therefore ignore my post as you are working with STM8.

Posted on January 05, 2017 at 08:55

Have you enabled the interrupts?

enableInterrupts();  // usally before the main while loop...

therefore you have to include: stm8l15x.h

ramon13666
Associate II
Posted on January 09, 2017 at 08:55

TIM1_CR1=0X81;
TIM1_IER=0X01;�?�?

Change to

TIM1_IER=0X01;
TIM1_CR1=0X81;�?�?