cancel
Showing results for 
Search instead for 
Did you mean: 

I want to insert some assembly language commands in my C-program. Say "nop". The compiler doesn't accept it in any form. I have tried various suggestions given on net. Can anyone please give me exactly what to type in program and how to define it.

KSahn.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7

Using what compiler?

Check the manual for "inline assembly/assembler"

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

https://lujji.github.io/blog/mixing-c-and-assembly-on-stm8/

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KSahn.1
Associate II

Thanks for the reply, Let me try it. So far I was using ATMEL. This is my first try with ST. I am using STVD with cosmic compiler. Meanwhile can you please check, whats wrong with this. It is giving error.

#include <stm8s103k.h>

#include <stm8.h>

#define LED_PORT  PD

#define LED_PIN   PIN3

static const _flash uint8_t Digits[4] = { 0B01111110, 0B00001100, 0B10110110, 0B10011110 };

int main(void) {

unsigned long count;

CLK_CKDIVR = 0B00001000;

   PORT(LED_PORT, DDR) |= LED_PIN; // i.e. PB_DDR |= (1 << 5);

   PORT(LED_PORT, CR1) |= LED_PIN; // i.e. PB_CR1 |= (1 << 5);

while(1) {

    PORT(LED_PORT, ODR) |= LED_PIN; // PB_ODR |= (1 << 5);

     count = 100000L;

while (count > 0)

{ count--; }

    PORT(LED_PORT, ODR) &= ~LED_PIN; // PB_ODR &= ~(1 << 5);

     count = 100000L;

while (count > 0)

{ count--; }

}

return(0);

}0693W000001rKsNQAU.jpg

Does it accept binary constants?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KSahn.1
Associate II

Yes it does. I used it again CLK_CKDIVR = 0B00001000; in line-12.

KSahn.1
Associate II

Sir, one more reason I might be overlooking. It is showing a message at startup. Can you please check this.0693W000001rLpjQAE.jpg

KSahn.1
Associate II

Dear Sir, I changed the settings to ST Assembler Linker instead of Cosmic, and it compiled well. No errors. Now can I program this file with S19 extension directly to my chip ????