cancel
Showing results for 
Search instead for 
Did you mean: 

I need help with CAN BUS Driver.

ASafo.8
Associate

Good day to all,

I have STM8Adiscovery and i'm trying to load example from StdPh for the Can Bus but it's not working at all. 

Development tool IAR for STM8. 

What I have - as i see from the beggining, program try to send data 2 times - and then Can bus start to be un active as i understand that because buffer of mailboxes is full. But in this time i don't any signals on the osciloscope.

For sniff CAN buss i'm using IXXAT USB-to-CAN compact - that tool also don't see any kind of messages. I checked several examples, tryed to configure by my self but still don't have working driver (((((

Could someone check my source codes and give some advices.

Thank you!

void CanDriver_Init( void )

{  

 CAN_InitStatus_TypeDef status = CAN_InitStatus_Failed;

  

 /* Filter Parameters */

 CAN_FilterNumber_TypeDef CAN_FilterNumber;

 FunctionalState CAN_FilterActivation;

 CAN_FilterMode_TypeDef CAN_FilterMode;

 CAN_FilterScale_TypeDef CAN_FilterScale;

 uint8_t CAN_FilterID1;

 uint8_t CAN_FilterID2;

 uint8_t CAN_FilterID3;

 uint8_t CAN_FilterID4;

 uint8_t CAN_FilterIDMask1;

 uint8_t CAN_FilterIDMask2;

 uint8_t CAN_FilterIDMask3;

 uint8_t CAN_FilterIDMask4; 

  

 /* Init Parameters*/

 CAN_MasterCtrl_TypeDef CAN_MasterCtrl;

 CAN_Mode_TypeDef CAN_Mode;

 CAN_SynJumpWidth_TypeDef CAN_SynJumpWidth;

 CAN_BitSeg1_TypeDef CAN_BitSeg1;

 CAN_BitSeg2_TypeDef CAN_BitSeg2;

 uint8_t CAN_Prescaler;  

  

 /* CAN register init */

 CAN_DeInit();

   

 /* CAN init */

 CAN_MasterCtrl=CAN_MasterCtrl_AllDisabled;

 CAN_Mode = CAN_Mode_Normal;

 CAN_SynJumpWidth = CAN_SynJumpWidth_1TimeQuantum;

 CAN_BitSeg1 = CAN_BitSeg1_8TimeQuantum;

 CAN_BitSeg2 = CAN_BitSeg2_7TimeQuantum;

 CAN_Prescaler = 1;

 status = CAN_Init(CAN_MasterCtrl, CAN_Mode, CAN_SynJumpWidth, CAN_BitSeg1, \

          CAN_BitSeg2, CAN_Prescaler);

 /* CAN filter init */

 CAN_FilterNumber = CAN_FilterNumber_0;

 CAN_FilterActivation = ENABLE;

 CAN_FilterMode = CAN_FilterMode_IdMask;

 CAN_FilterScale = CAN_FilterScale_32Bit;

 CAN_FilterID1=0;  

 CAN_FilterID2=0;

 CAN_FilterID3=0;

 CAN_FilterID4=0;

 CAN_FilterIDMask1=0;

 CAN_FilterIDMask2=0;

 CAN_FilterIDMask3=0;

 CAN_FilterIDMask4=0;  

 CAN_FilterInit(CAN_FilterNumber, CAN_FilterActivation, CAN_FilterMode, 

         CAN_FilterScale,CAN_FilterID1, CAN_FilterID2, CAN_FilterID3,

         CAN_FilterID4,CAN_FilterIDMask1, CAN_FilterIDMask2, 

         CAN_FilterIDMask3, CAN_FilterIDMask4);

     

 /* Enable Fifo message pending interrupt*/

 /* Message reception is done by CAN_RX ISR*/

 CAN_ITConfig(CAN_IT_FMP, ENABLE);

}

---------------------------

INTERRUPT_HANDLER(CAN_RX_IRQHandler, 8)

{

 // Receiver Receives Frame

 CAN_Receive();

}

----------------------------

void CanDriver_Process( void )

{  

  

 CAN_TxStatus_TypeDef status = CAN_TxStatus_Failed;

  

 /* Transmit Parameters */

 CAN_Id_TypeDef Tx_IDE = CAN_Id_Standard;

 CAN_RTR_TypeDef Tx_RTR = CAN_RTR_Data;

 uint8_t Tx_DLC = 0;

 uint8_t Tx_Data[8] = {0};

 uint32_t Tx_Id = 0; 

  

 // Transmit Parameters

 Tx_Id = 0x321;

 Tx_IDE = CAN_Id_Standard;

 Tx_RTR = CAN_RTR_Data;

 Tx_DLC = 1;

 Tx_Data[0] = 0xAA;    

 Tx_Data[1] = 0x11;

 Tx_Data[2] = 0xBB;

 Tx_Data[3] = 0x22;

 Tx_Data[4] = 0xCC;

 Tx_Data[5] = 0x33;

 Tx_Data[6] = 0xDD;

 Tx_Data[7] = 0x44;

 // Sender send Frame

 status = CAN_Transmit(Tx_Id,Tx_IDE,Tx_RTR,Tx_DLC,Tx_Data);

}

For CLK

void CLK_Init(void)

{

  CLK_DeInit();

   

  CLK_HSECmd(ENABLE);

  /* Configure the Fcpu to DIV1*/

  CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);

  /* Output Fcpu on CLK_CCO pin */

  CLK_CCOConfig(CLK_OUTPUT_HSE);

  /* Configure the system clock to use HSE clock source and to run at 16Mhz */

  CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSE, DISABLE, CLK_CURRENTCLOCKSTATE_DISABLE);

   

  CLK_PeripheralClockConfig( CLK_PERIPHERAL_TIMER1, ENABLE);

  CLK_PeripheralClockConfig( CLK_PERIPHERAL_TIMER3, ENABLE);

  CLK_PeripheralClockConfig( CLK_PERIPHERAL_CAN, ENABLE);

}

For GPIO

 // CAN_TX

GPIO_Init( GPIOG, GPIO_PIN_0, GPIO_MODE_OUT_PP_HIGH_FAST );

// CAN_RX

GPIO_Init( GPIOG, GPIO_PIN_1, GPIO_MODE_IN_PU_NO_IT );

   

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0