2021-06-03 4:01 AM
Compiling main.c...
cxstm8 +warn +mods0 +debug -pxp +strict -pp -ps -psa -pu -l -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\Hstm8" -clDebug\ -coDebug\ main.c
#error cpstm8 stm8s.h:2525(12) missing ;
#error cpstm8 stm8s_gpio.h:68(18) incomplete declaration
#error cpstm8 stm8s_gpio.h:141(61) bad proto argument type
#error cpstm8 stm8s_gpio.h:141(53+8) missing )
#error cpstm8 stm8s_gpio.h:141(91) missing ;
#error cpstm8 main.c:44(28+21) too many arguments
#error cpstm8 main.c:45(28+21) too many arguments
#error cpstm8 main.c:46(28+21) too many arguments
#error cpstm8 main.c:47(55) too many arguments
#error cpstm8 main.c:48(28+21) too many arguments
#error cpstm8 main.c:47(29+26) GPIO_MODE_OUT_PP_HIGH_FAST undefined
#error cpstm8 main.c:44(28+21) GPIO_MODE_IN_PU_NO_IT undefined
main.c:
The command: "cxstm8 +warn +mods0 +debug -pxp +strict -pp -ps -psa -pu -l -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\Hstm8" -clDebug\ -coDebug\ main.c" has failed, the returned value is: 1
exit code=1.
2021-06-03 4:50 AM
I have used same gpio files in earlier project, at that time there was no errors.
I am using cosmic 8 compiler in stvd.
Error corresponding to line is as follows:
too many arguments , undefined
GPIO_Init(GPIOD,GPIO_PIN_4,GPIO_MODE_IN_PU_NO_IT);
GPIO_Init(GPIOC,GPIO_PIN_5,GPIO_MODE_IN_PU_NO_IT);
GPIO_Init(GPIOC,GPIO_PIN_6,GPIO_MODE_IN_PU_NO_IT);
GPIO_Init(GPIOC,GPIO_PIN_7,(GPIO_MODE_OUT_PP_HIGH_FAST));
GPIO_Init(GPIOA,GPIO_PIN_3,GPIO_MODE_IN_PU_NO_IT);
#error cpstm8 stm8s_gpio.h:141(61) bad proto argument type
void GPIO_WriteLow(GPIO_TypeDef* GPIOx, GPIO_Pin_TypeDef PortPins);
#error cpstm8 stm8s_gpio.h:141(53+8) missing )
#error cpstm8 stm8s_gpio.h:141(91) missing ;
void GPIO_WriteLow(GPIO_TypeDef* GPIOx, GPIO_Pin_TypeDef PortPins);
2021-06-03 4:54 AM
Also I have many times that compiler gives error inspite of everything is correct.
Is there any specific setting that we have to do in stvd if unnecesssary are prompted.