cancel
Showing results for 
Search instead for 
Did you mean: 

How to use UART at STM8L050j3?

KTAEW.1
Associate

Hello,

Using STM8L050j3, ST LINK/V2 ISOL, STVD.

I am studying the UART and i have connected MCU and ST LINK/V2 ISOL.

They use SWIM with USART TX / RX Pin.

A problem is that PC don't receive the any text.​

I think that cording is fine(easy example) but i suspect that the PC and MCU are properly connected.

Checked the USART parameters(Baudrate,Wordlength,stopbits,Parity...) on S/W and cording.

Used the various terminal S/W.

Swaped the MCU.

Please let me know how to use UART.

best regards.

-- cord --

#include "stm8l15x.h"

#ifdef _RAISONANCE_

#define PUTCHAR_PROTOTYPE int putchar (char c)

#define GETCHAR_PROTOTYPE int getchar (void)

#elif defined (_COSMIC_)

#define PUTCHAR_PROTOTYPE char putchar (char c)

#define GETCHAR_PROTOTYPE char getchar (void)

#else /* _IAR_ */

#define PUTCHAR_PROTOTYPE int putchar (int c)

#define GETCHAR_PROTOTYPE int getchar (void)

#endif /* _RAISONANCE_ */

void delay(uint16_t n);

void main(void)

{

 char ans;

delay(300);

 CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1);

CLK_PeripheralClockConfig(CLK_Peripheral_USART1,ENABLE);

GPIO_Init(GPIOC,GPIO_Pin_5,GPIO_Mode_Out_PP_High_Fast);

GPIO_Init(GPIOC,GPIO_Pin_6,GPIO_Mode_In_PU_No_IT);

GPIO_ExternalPullUpConfig(GPIOC,GPIO_Pin_5 | GPIO_Pin_6,ENABLE);

 USART_Init(USART1, (uint32_t)115200, USART_WordLength_8b, USART_StopBits_1, USART_Parity_No, (USART_Mode_TypeDef)(USART_Mode_Tx | USART_Mode_Rx));

GPIO_Init(GPIOB, GPIO_Pin_6 | GPIO_Pin_5 , GPIO_Mode_Out_PP_Low_Slow);

USART_Cmd(USART1, ENABLE);

 while(1)

 {

  GPIO_ToggleBits(GPIOB, GPIO_Pin_5);

delay(100);

USART_SendData8(USART1, 'A');

  //ans = getchar();

}

}

PUTCHAR_PROTOTYPE

{

 /* Write a character to the USART */

 USART_SendData8(USART1, c);

 /* Loop until the end of transmission */

 while (USART_GetFlagStatus(USART1, USART_FLAG_TC) == RESET);

 return (c);

}

GETCHAR_PROTOTYPE

{

 int c = 0;

 /* Loop until the Read data register flag is SET */

 while (USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET);

  c = USART_ReceiveData8(USART1);

  return (c);

 }

void delay(uint16_t n)

{

  uint16_t i,j;

  for (i=0; i<n; ++i) {

   for (j=0; j<3050; ++j) { _asm("nop"); } 

  }

}

#ifdef USE_FULL_ASSERT

 void assert_failed(uint8_t* file, uint32_t line)

 {

  while (1)

  {}

 }

#endif

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
dbgarasiya
Senior II

should be enable interrupt