cancel
Showing results for 
Search instead for 
Did you mean: 

How to design NEC IR decoder in STM8S103F3 ?

jeffrey2
Associate II
Posted on January 07, 2010 at 09:33

How to design NEC IR decoder in STM8S103F3 ?

#remote #nec #ir
This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
jeffrey2
Associate II
Posted on May 17, 2011 at 15:06

I am designing a battery-based device.

It stayed power down mode normally and

is powered on by NEC remoter controller.

Are there any STM8S103 reference design or

technical information for reference ?

Thanks in advance !

st3
Associate II
Posted on May 17, 2011 at 15:06

Quote:

Are there any STM8S103 reference design or technical information for reference ?

It's all here:

http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=113

 

jeffrey2
Associate II
Posted on May 17, 2011 at 15:06

Quote:

On 15-12-2009 at 10:15, Anonymous wrote:

Quote:

Are there any STM8S103 reference design or technical information for reference ?

It's all here:

http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=113

 

Are there any application notes which describe the TV NEC IR decoder

design in STM8S MCU ?

mozra27
Associate II
Posted on May 17, 2011 at 15:06

Hi Jeffrey,

You can refer to the ''AN2957: Implementing an RC5 infrared transmitter using the IR timer modulator of the STM8L10x microcontroller'' available in this link:

http://www.st.com/mcu/familiesdocs-120.html

This Appli note use the IRTIM IP that is not available on the STM8S products family but can be updated using the Timer ;)

regards

mozra

selva
Associate II
Posted on May 17, 2011 at 15:06

Hi Jeffrey,

You want to implement an IR transmitter? or receiver?

regards

skuk

jeffrey23
Associate II
Posted on May 17, 2011 at 15:06

I had implemented the NEC IR receiver using PC.6,

but it may be conflicted with other signal (PC.3).

They shared the same EXTI_PORTC_ISR

interrupt service routine. How to distinguish them

in ISR ?

selva
Associate II
Posted on May 17, 2011 at 15:06

Hi,

Am new to STM8 family! and my plan to use Timer1 function to decode NEC IR pulses is on hold for the below reason:

 

I configured myself every register according to ref manual RM0016 (14587.pdf), section 17.5.3.

Also have chosen PIO config as alternate input with interrupt on DDR, CR1, CR2.

There is an interrupt raised on press of the key, but the CC1IF bit is not set, instead, the register is always 0x19, which is to say CC4IF, CC3IF.

That didn’t help!

I managed to dig out the reference code on timer, stm8s_tim1.c, and used that as well. Still the same effect

This makes me think, perhaps I have missed to set/reset just “one bit� somewhere!

If you could share me your thoughts and further check points or some source code to refer to, that would be appreciated.

Many thanks,

Skuk.
krzysio
Associate
Posted on May 17, 2011 at 15:06

Hi Boltnut,

are you writing in C or ASM?

could you show me your code?

i'm working on rc receiver too?

jeffrey23
Associate II
Posted on May 17, 2011 at 15:06

Hi wojcik.krzysztof,

I had implemented the NEC IR decoder (PC.6) in STM8S103F3, but

it is disturbed by other signal (PC.3). So far I do NOT know

how to distinguish the EXTI Port C pins interrupt sources to overcome

the issue.