cancel
Showing results for 
Search instead for 
Did you mean: 

Hello everyone, what does JRT instruction, and which difference among JRT and JP instructions? Thank you!

flankerus
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Philipp Krause
Senior III

Well, there is table 42 with the descriptions. The one for jrf states "never jump". The instruction set entry for nop (which is separate from jrf states "see also: jrf").

It might be there for orthogonality. The reasoning for including such an instruction in the HC08 / S08 architecture was that the jrf can be used as a placeholder for a jra to some debug instrumentation code (so the debug build would have the same code locations as the non-debug build).

An interesting aspect of jrf is that it is essentially a two-byte nop for any second byte. If you put a valid 1-byte instruction into the 2nd byte, you could see jrf as a jump over that 1-byte instruction (saving 1 byte over using a jra). That can be useful in a if/else, where the else consists of just a 1-byte instruction. SDCC actually uses jrf for such an optimization.

Philipp

View solution in original post

4 REPLIES 4
Philipp Krause
Senior III

jrt (which is more commonly called jra) is a relative jump instruction. It can only jump to nearby targets, takes 2 bytes and 2 cycles. jp is an absolute jump, that can jump to anywhere within a 16-bit address space. It takes 3 bytes and 1 cycle.

So in cases where you could use either it is a trade-off between code size and speed.

For more details see the "STM8 CPU programming manual":

https://www.st.com/resource/en/programming_manual/cd00161709.pdf

Philipp

flankerus
Associate II

Yes, it's understandable. I read the manual, but unfortunately it is very short.

I thought a lot about what a would mean to False or True in the "Condition" column for instructions JRT and JRF.

Ok, JRT it's alias for JRA. 

What is JRF? Alias for NOP? 

Philipp Krause
Senior III

Well, there is table 42 with the descriptions. The one for jrf states "never jump". The instruction set entry for nop (which is separate from jrf states "see also: jrf").

It might be there for orthogonality. The reasoning for including such an instruction in the HC08 / S08 architecture was that the jrf can be used as a placeholder for a jra to some debug instrumentation code (so the debug build would have the same code locations as the non-debug build).

An interesting aspect of jrf is that it is essentially a two-byte nop for any second byte. If you put a valid 1-byte instruction into the 2nd byte, you could see jrf as a jump over that 1-byte instruction (saving 1 byte over using a jra). That can be useful in a if/else, where the else consists of just a 1-byte instruction. SDCC actually uses jrf for such an optimization.

Philipp

flankerus
Associate II

>An interesting aspect of jrf is that it is essentially a two-byte nop for any second byte.

Curious. The Reference Manual for HCS08 for the BRN has a more detailed description:

"This instruction can be useful in instruction-based timing delays. Instruction-based timing delays are

usually discouraged because such code is not portable to systems with different clock speeds."

Does this have a relationship with STM8? I don't understand how to make a delay on the basis of JRF or BRN instruction.

   ;code of delay 1sec without JRF:
stm8/
    segment 'rom'
   ; delay 1 sec, when fCPU=2MHz
.delay:
    ld a, #$06
    ldw y, #$1a80             ; 0x61a80 = 400000 i.e. (2*10^6 MHz)/5cycles
loop:
    subw y, #$01             ; 2 cycles
    sbc a,#0                      ; 1 cycles
    jrne loop		         ; 2 cycles, flush
    ret
    end

code of delay 1sec with JRF:

stm8\
	segment 'rom'
	; delay 1 sec, when fCPU=2MHz
.delay:
	ld a, #$03
	ldw y, #$d090               ; 0x3d090=250000(dec)  i.e. (2*10^6 MHz)/8cycles
loop:  
	subw y, #$01                ; =2 cycles
	sbc a,#0                         ; =1 cycles
	jreq {exit+1}                  ; =1 cycles
exit:  
	dc.b $21, $81               ; JRF RET, =2 cycles, flush
	jra loop                          ; =2 cycles, flush
	end

It's has meaning?