2019-08-22 3:20 AM
Hello,
I'm starting to use the STM8L family and in particular the STM8L050 MCU. I want to start with low power so i wrote this piece of code :
/* MAIN.C file
*
* Copyright (c) 2002-2005 STMicroelectronics
*/
#include <stdint.h>
#include "stm8l.h"
#define LED1_PORT PC
#define LED1_PIN PIN1
#define LED2_PORT PA
#define LED2_PIN PIN3
#define LED3_PORT PB
#define LED3_PIN PIN6
#define LED4_PORT PB
#define LED4_PIN PIN3
/* Simple busy loop delay */
void delay(unsigned long count)
{
while (count--)
nop();
}
void init_gpio(void)
{
/* GPIO setup */
/*
// Set pin data direction as output
PORT(LED1_PORT, DDR) |= LED1_PIN; // i.e. PB_DDR |= (1 << 5);
// Set pin as "Push-pull"
PORT(LED1_PORT, CR1) |= LED1_PIN; // i.e. PB_CR1 |= (1 << 5);
*/
PORT(LED2_PORT, DDR) |= LED2_PIN; // i.e. PB_DDR |= (1 << 5);
// Set pin as "Push-pull"
PORT(LED2_PORT, CR1) |= LED2_PIN; // i.e. PB_CR1 |= (1 << 5);
/*
PORT(LED3_PORT, DDR) |= LED3_PIN; // i.e. PB_DDR |= (1 << 5);
// Set pin as "Push-pull"
PORT(LED3_PORT, CR1) |= LED3_PIN; // i.e. PB_CR1 |= (1 << 5);
PORT(LED4_PORT, DDR) |= LED4_PIN; // i.e. PB_DDR |= (1 << 5);
// Set pin as "Push-pull"
PORT(LED4_PORT, CR1) |= LED4_PIN; // i.e. PB_CR1 |= (1 << 5);
*/
}
main()
{
// Secure delay for flashing
delay(100000L);
/* Set clock to full speed (16 Mhz) */
//CLK_CKDIVR = 0;
init_gpio();
while(1) {
// LED on
PORT(LED2_PORT, ODR) |= LED2_PIN; // PB_ODR |= (1 << 5);
delay(10000L);
// LED off
PORT(LED2_PORT, ODR) &= ~LED2_PIN; // PB_ODR &= ~(1 << 5);
delay(10000L);
// enter SLEEP mode
wfi();
}
}But it seems to go in sleep mode but i cannot reach the current target. I'm still consuming arround 330mA and i don't know why. Am i missing something with the clock ?
Here is my schematics which is very simple as well. I only soldered the MCU with the decoupling capacitors.
If you have any indication, feel free to share.
Best regards,
Aurélien