cancel
Showing results for 
Search instead for 
Did you mean: 

BLDC sensor based Motor control with the STM8S

dominik2399
Associate II
Posted on January 12, 2010 at 14:13

BLDC sensor based Motor control with the STM8S

5 REPLIES 5
dominik2399
Associate II
Posted on May 17, 2011 at 15:03

Hello

I'm searching a motor control library to control a BLDC motor with hall sensors and direct communtation. I'm working on a STM8S and need this library or C-Code as soon as possible. Can you help me? Or do you have a library for the STM32 or another type, so I can modify the code for the STM8S.

Thanks a lot

Regards, Dominik

abelmeg
Associate II
Posted on May 17, 2011 at 15:03

The library you're looking for is found at

http://www.st.com/stonline/products/support/micro/files/stm8mcfwlib.zip

regards..

m_kisacanin
Associate II
Posted on May 17, 2011 at 15:03

Is this supposed to be an (Windows) executable?

Libraries usually come as ''bunch of .h and .c'' in a clear text/folder structure.

Not that I'm paranoid (well I am), but don't like running someone's else exe on my machine :)

abelmeg
Associate II
Posted on May 17, 2011 at 15:03

Its not .exe. It is Zipped file containing .h .c and workspace files. If you want to know more about the library look

http://www.st.com/stonline/products/literature/um/15773.pdf

regards.

m_kisacanin
Associate II
Posted on May 17, 2011 at 15:03

The file comes as a zip archive, but inside the archive is

STM8MC-KIT_1.0_090703.exe file (executable as mentioned before).