STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

No NRST pin, How to program STM8S001J3M with SWIM interface,

Hi,I want to program STM8S001J3M with SWIM interface, and the device doesn't have NRST pin, I see in the datasheet there is :Only the “connect on-the-fly�? method can be used to program the device through the SWIM interface. The “connect under-reset�...

XLi.3 by Associate II
  • 1517 Views
  • 2 replies
  • 0 kudos

how to reduce offset voltage

Hiii,i am using STM8s003f3 controller. i am trying to measure DC voltage but got some offset error on display and because of this error i am not getting 0000 value on display when there is no input is connected.how can get rid of this error in C,is ...

MAnsa.1 by Associate II
  • 823 Views
  • 1 replies
  • 0 kudos

i need to learn STM8Sxxxx

please anybody can help me i want to learn STM8Sxxxx i only know Gpio's and interrupt controlling please provide lecture or material sources

AALAM.1 by Associate
  • 816 Views
  • 2 replies
  • 1 kudos

STM8AF6266TCX linker input settings

We are migrating MCU from STM8AF6246TASSSX to STM8AF6266TCX.Since we are observing issue in LINKER input setting . Though we are able to compile , we are missing part of code . We appreciate quick response.

BSidd.1 by Associate II
  • 628 Views
  • 0 replies
  • 0 kudos

Stm8s spi fill duplex master multi-byte transfers

Hi,I have been trying to interface stm8s003k3 with and external ic ​using spi in full duplex master mode .I have been successful to set up the spi in full duplex master mode but the part where recieving and transfering data becomes tricky and I have ...

0693W000008GEWyQAO.jpg 0693W000008GEX3QAO.jpg 0693W000008GEX8QAO.jpg 0693W000008GEYfQAO.jpg
CClas.1 by Associate
  • 2092 Views
  • 1 replies
  • 1 kudos

Linker setting for STM8AF6266TCX MCU . We are migrating MCU from STM8AF6246TASSSX to STM8AF6266TCX. Note : We are retaining same Source code in both projects.

I am observing LINKER error during project build .#error clnk Debug\jlrmemoryswitch.lkf:1 can't locate checksum segment#error clnk Debug\jlrmemoryswitch.lkf:1 segment .ubsct size overflow (85)#error clnk Debug\jlrmemoryswitch.lkf:1 no default placeme...

BSidd.1 by Associate II
  • 600 Views
  • 0 replies
  • 0 kudos