STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S003k3 EXTI interrupt double entering problem

Posted on May 22, 2015 at 18:54 Hello i have some problem withSTM8S003k3 and IR recieve protocol. I set EXTI PORTB interrupt by RISE and FALL: GPIO_DeInit(GPIOB); GPIO_Init(GPIOB, GPIO_PIN_2, GPIO_MODE_IN_FL_IT); disableInterrupts(); EXTI...

STM8S: cannot communicate with ROM Bootloader!

Posted on May 11, 2015 at 14:12Hi, we are trying to program a STM8S-Discovery, fitted with a STM8S105x6 microcontroller, using the native bootloader (via USART1 pins). We disconnetted the onboard ST-Link by removing R13-R14 resistor. We are usin...

STM8S003F3 Timer Issue

Posted on May 20, 2015 at 23:52Hey guys, I recently wrote some code to turn on Timer1 channels 1-3 and Timer2 channel 1 as PWMs to pulse a few LEDs. This code was originally written for the STM8S003K3, but I am now trying to switch over to an STM8S0...

cfleck by Associate II
  • 621 Views
  • 0 replies
  • 0 kudos

STM8L MCU interface to ST-LINK/V2 programmer

Posted on April 30, 2015 at 01:32First time using an STM8L MCU.  I am drawing a schematic and I am not sure if my programming connector is wired right.  I will use an ST-LINK/V2 programmer.  Do I simply connect the 4-pin connector as shown below?  P...

0690X00000602m6QAA.jpg
jmm385 by Associate
  • 915 Views
  • 2 replies
  • 0 kudos

STM8S003k3 TIM1 PWM problem

Posted on May 08, 2015 at 15:44Hello every one. I have a workable code of pwm on STM8S105K4T6 and now I paste it in STM8S003k3 fnd it won't work.&sharpdefine CCR1_Val  ((u16)2047) // Configure channel 1 Pulse Width Blue&sharpdefine CCR2_Val  ((u16)2...

STVD: Preserve EEPROM

Posted on May 05, 2015 at 15:59How can I preserve the EEPROM contents when debugging my application on the STM8S003?I use STVD and either the STLink/V2 or the RLink.

Implement one wire slave ?

Posted on January 30, 2013 at 15:12Please can you tell me how to implement one wire slave in stm8s ?Note: the one wire master is GPS TELTONIKA FM1100 #1-wire

STM8S003F3U programming

Posted on April 16, 2015 at 14:04I'm totally new to STM8 microcontroller series. I'm planning to do a project using STM8S003F3U controller in which ADC and timer module will be used. It would be useful if i could find some sample codes for ADC,timer...

Debugging problem of STM8

Posted on April 30, 2015 at 08:21I'm doing a project on STM8S003F3. Im using IAR instead of stvd for developmeant purpose. I could create my sample project and successfully debugged it. It was working fine for few days. But today debug session termi...

STM8 startup bug Timer 2 input capture

Posted on April 28, 2015 at 12:50 Hi, I wanna make a frequency pulse counter with an STM8. The counter is based on the input capture of the STM timer 2. The frequency is a frequency with a range of 1 Hz - 20 kHz. With the following ...

mitchell by Associate
  • 628 Views
  • 0 replies
  • 0 kudos