STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STVD Software is not responding

Hi, I am using ST Visual Develop environment for programming of STM8S207, i am using 4.3.6 version. Problem is, whenever i give save command, STVD is halt and shown "Not Responding" My laptop configuration is Pentium Dual Core, 2.0GB RAM, Window ...

Resolved! Issue reading program data from the flash

Good afternoon, I would like to share an issue I’m facing with a stm8s105c4.A feature of our main application is to calculate a CRC of the entire program in the flash. Unfortunately, when I read flash data from addresses close to the instruction in e...

0690X000006D6h8QAC.png 0690X000006D6hDQAS.png 0690X000006D6hIQAS.png 0690X000006D6hNQAS.png

Cursor alway run to EXTI line when hold press button

Hi all,I have a issue about interrupt timer and interrupt button. When i alway press button. Run debug, cursor alway run to interrupt exti line. I change timer 2,4 or pin exti still error occur. When I comment TIM1_Config() i alway press button-->in...

TMai by Associate
  • 770 Views
  • 2 replies
  • 1 kudos

Free IDE for STM8 development

HI ST Team,We are planning to use STM8S103F2 MCU for dimmer application like the STEVAL-ILD004V2 reference board. Do you have IDE we can use (for free) or we need to get Keil/IAR license?Regards,Walter

WMaca by Associate II
  • 1467 Views
  • 6 replies
  • 0 kudos

What is #error cgstm8 .... PANIC! MOVCNT

What is the meaning and root cause of following error:#error cgstm8 xsnprintf.c:195 >123<@generate() PANIC! MOVCNTI am trying to build a custom printf routine. This shows up only after I change the type of some parameters.

MRodr.12 by Associate
  • 590 Views
  • 1 replies
  • 0 kudos

Hello, i'm searching for the Source Code for the Eval Board STEVAL-ILD004V2? There is only the compiled Firmware Version. Can anybody help me?

Posted on November 17, 2017 at 14:08Hello,i'm searching for the Source Code of the EVAL Board STEVAL-ILD004V2 with STM8S103F2 Controller?I can only found the compiled Firmware.Can anybody help me?Best Regards,Stefan#steval-ild004v2-source-code?

Resolved! What MC is this? And how to transfer code to another chip?

The image below, is of a SNES Classic (Super Nintendo Classic) controller's PCB. I can't seem to find out exactly what MC its using, all it really says is STM8mhz. On LCSC and digikey, they don't even have any 8mhz STM8 MCs, only 16 and 24mhz. This i...

0690X000006D3sSQAS.jpg
AOlth by Associate
  • 740 Views
  • 2 replies
  • 0 kudos