ADC1 with with COMP1?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-08-21 12:18 PM
Posted on August 21, 2014 at 21:18
Hello,
I am working on an application which requires the use of the ADC1 peripheral as well as the COMP1 & COMP2 peripherals. There does not appear to be anything in the datasheet against this, but there is a note in the comparator driver:''COMP1 comparator and ADC can't be used at the same time since they share the same ADC switch matrix (analog switches).'' -stm8l15x_comp.c
Is this a limitation of the driver, or of the chip? If it is a chip limitation, could someone please point me in the direction of the datasheet that mentions it? If it is a driver limitation, does anyone know if there is there a work-around?Thanks!Gabrielle
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0