cancel
Showing results for 
Search instead for 
Did you mean: 

Accessing EEPROM with Cosmic compiler

jark
Associate II
Posted on July 26, 2010 at 20:46

Accessing EEPROM with Cosmic compiler

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
luca239955_stm1_st
Senior II
Posted on May 17, 2011 at 15:09

Hi,

there's no need for include files, but you must define a .eeprom segment in the linker file (I'm not sure if STVD does that automatically).

What linker error do you have exactly?

Regards,

Luca

jark
Associate II
Posted on May 17, 2011 at 15:09

Hi,

    Thanks for the quick response.  The error message I get is:

#error clnk Debug\lc_meter_v1.lkf:1 bad address (0x4000) for zero page symbol _Cstd

 The command: ''clnk -l''C:\Program Files\COSMIC\CXSTM8_16K\Lib''  -o Debug\lc_meter_v1.sm8 -l..\..\..\..\libraries\stm8s_stdperiph_driver -mDebug\lc_meter_v1.map Debug\lc_meter_v1.lkf '' has failed, the returned value is: 1

exit code=1.

    Thanks,

    Jim

luca239955_stm1_st
Senior II
Posted on May 17, 2011 at 15:09

looks like something is wrong with your linker file, please post it.

jark
Associate II
Posted on May 17, 2011 at 15:09

OK - here's the file

# LINK COMMAND FILE AUTOMATICALLY GENERATED BY STVD: TOTALLY

# IF AUTO MODE IS ENABLED, OR ONLY PARTIALLY WHEN AUTO MODE

# IS DISABLED (see below).

#

# CAUTION:

#

# Sections delimited by <BEGIN ...> and <END ...> markers are

# reserved for STVD: DO NOT MODIFY INSIDE.

#

# Manual modifications are allowed OUTSIDE these sections, WHEN

# STVD ''auto'' MODE IS DISABLED (if ''auto'' mode is enabled,

# modifications are lost).

# When STVD ''auto'' mode is disabled, it is also possible to disable

# the automatic update inside the reserved sections, by removing the

# <BEGIN ...> and <END ...> markers of the corresponding section.

#

# Please refer to Cosmic User Manuals before any modification.

# Note that errors in editing this file may have unpredictable results

# when running STVD.

# Segment configuration - section reserved for STVD

#<BEGIN SEGMENT_CONF>

# Segment Code,Constants:

+seg .const -b 0x8080 -m 0x7f80 -n .const -it

+seg .text -a .const -n .text

# Segment Eeprom:

+seg .eeprom -b 0x4000 -m 0x400 -n .eeprom

# Segment Zero Page:

+seg .bsct -b 0x0 -m 0x100 -n .bsct

+seg .ubsct -a .bsct -n .ubsct

+seg .bit -a .ubsct -n .bit -id

+seg .share -a .bit -n .share -is

# Segment Ram:

+seg .data -b 0x100 -m 0x500 -n .data

+seg .bss -a .data -n .bss

#<END SEGMENT_CONF>

# Startup file - section reserved for STVD

#<BEGIN STARTUP_FILE>

crtsi0.sm8

#<END STARTUP_FILE>

# Object files list - section reserved for STVD

#<BEGIN OBJECT_FILES>

Debug\stm8s_clk.o

Debug\stm8s_gpio.o

Debug\stm8s_itc.o

Debug\main.o

Debug\stm8_interrupt.o

Debug\stm8s_adc1.o

Debug\stm8s_beep.o

Debug\stm8s_exti.o

Debug\stm8s_lcd.o

Debug\stm8s_tim1.o

Debug\stm8s_tim2.o

Debug\stm8s_tim3.o

Debug\stm8s_tim4.o

Debug\timers.o

Debug\utilities.o

#<END OBJECT_FILES>

# Library list - section reserved for STVD

#<BEGIN LIBRARY_FILES>

libfs0.sm8

libis0.sm8

libm0.sm8

#<END LIBRARY_FILES>

# Interrupt vectors file - section reserved for STVD

#<BEGIN VECTOR_FILE>

+seg .const -b 0x8000 -k

Debug\stm8_interrupt_vector.o

#<END VECTOR_FILE>

# Defines - section reserved for STVD

#<BEGIN DEFINED_VARIABLES>

+def __endzp=@.ubsct            # end of uninitialized zpage

+def __memory=@.bss                # end of bss segment

+def __startmem=@.bss

+def __endmem=0x5ff

+def __stack=0x7ff

#<END DEFINED_VARIABLES>

jark
Associate II
Posted on May 17, 2011 at 15:09

Hi,

   I may have found the problem.  I used Cstd in both the main.c module and also in another module of the program.  There, I referred to it as:

extern float Cstd;

If I referred to it as 'extern @eeprom float Cstd', I got an error; I did not get an error if I referred to it as shown above.

    I only used it in one procedure there and have just found that, if I move that procedure into my main.c module where I declare all the variables, I no longer get a clink error.  I have yet to determine if I can properly access Cstd in the program.  It is only written to in a calibration procedure which is only used infrequently - but it is read in many different places in the project.

luca239955_stm1_st
Senior II
Posted on May 17, 2011 at 15:09

the linker file looks correct, so that's not yet enough information to understand the problem..

This symbol that is giving the error ''Cstd'', is that something you defined?

Can I see the definition ? Or you can post the entire project of it not confidential

jark
Associate II
Posted on May 17, 2011 at 15:09

There's nothing confidential about the project but it is, I think, too long to post

the whole thing.  The section where I define the variables is:

// global variables follow

enum menu_t menu_mode;

enum meas_t measurement_mode;

float Cstd = 469.0e-12;

float C1 = 509.0e-12;

float L68 = 67.0e-6;

float L1 = 68.0e-6;

float Cx, Lx;

long f1, f2;

u8 s[16];

float rho;

char cont;

As above, it compiles, links and runs correctly.  I get the clink error when I change the line with Cstd in it to the following:

@eeprom float Cstd = 469.0e-12;

    Jim

jark
Associate II
Posted on May 17, 2011 at 15:09

Hi again,  OK, it compiles without errors and the program can read the value of Cstd when it is declared:

@eeprom float Cstd = 469.0e-12;

It is read frequently in the program.  However, in a calibration routine, if I try to change it with a statement like:

    Cstd = Cstd * 0.998;

it does not change - I read it a few lines later and it has just got the same value as initialized in the statement which defines the variable.

    Jim

jark
Associate II
Posted on May 17, 2011 at 15:09

 Hi,

    I've looked at the assembler code produced by the compiler for the brief code; it looks fine to me but it illustrates the problem.

 352                     ; 187                                                        Cstd = Cstd * factor;

 354  0141 ae0000            ldw    x,#_Cstd

 355  0144 cd0000            call    c_ltor

 357  0147 ae0075            ldw    x,#L531

 358  014a cd0000            call    c_fmul

 360  014d ae0000            ldw    x,#_Cstd

 361  0150 cd0000            call    c_eewrl

 

It looks like it reads the eeprom, does the multiplication and then tries to store it

back in eeprom with the call to c_eewrl.  However, when I run the program, the value in Cstd is NOT changed.

   Anyone have any suggestions?

   Jim