2010-03-11 7:56 AM
hiya,
just received this trying to get the stm32 board going with the dev tools......simple questions as doc is very lite. download etc is via st-link or usb on the stm32 eval baord ? trying to run this from virtual box as my work system is in production with another dev environment for the mcu we are currently using. that environment uses a ftdi driver which works fine, but not willing to compromise it for an eval! Is ther any starter documentation anywhere? Dave2010-03-11 10:00 AM
ok, getting somewhere, disconnect ub from mini stm32 pcb, move jumper near st-link debugger cable recycle power, frm iar can now debug/download project
gpio example ok, but joystick saying corrupt. I can see the libraries includes etc have usb drivers but nothing eventuating at the pc, not sure if there's a console back to the PC from st-link or mini board sfm32....but nothing being picked up so not sure if the drivers for fdti are working....... since doing the debug the deg server in atripllis now starts so might pursue that from hyper term tormoow. I knw the tools are free reduced versions but some doco would start would help dave