Master Clock Output issue
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-11-12 11:34 AM
Posted on November 12, 2016 at 20:34
I configured RCC Master Clock Output within cubeMX 4.0 and using a STM32F
The generated Code does not output the selected clock. I have found, after code analysis of generated file gpio.c, that the Alternate function for PA8 in MX_GPIO_Init() is not as expected./*Configure GPIO pin : PA8 */
GPIO_InitStruct.Pin = GPIO_PIN_8; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate =GPIO_AF0_TRACE;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);After changing the Alternate Function of PA8 to
GPIO_InitStruct.Alternate =
GPIO_AF0_MCO;
the Master Clock Output works as expected.
Regards AB
cubemx stm32f303
Labels:
- Labels:
-
STM32CubeMX
-
STM32F3 Series
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-11-14 6:17 AM
Posted on November 14, 2016 at 15:17
Hello,
Referring to the : PA8 is configured as AF0: MCO Alternate Function. The specific alternate function assignments for each pin are detailed in the device datasheet, ''Table Alternate functions''and ''Table STM32F303x6/8 pin definitions''. I have checked from my side and Icannot reproduce this issue (attached .ioc file).Could you please share your .ioc to check with you this case.
Regards ________________ Attachments : rcc.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HteS&d=%2Fa%2F0X0000000aSE%2Fhn5mmstvKoW06GL1oHpXRe_FIlCRrbFJ2hzGxULa03U&asPdf=falseOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-11-15 11:04 PM
Posted on November 16, 2016 at 08:04
Hello,
I re-tested and now the MCO output works. The problem was the speed setting of the pin. It seems to be all right now.
Thank you very much.
Regards