cancel
Showing results for 
Search instead for 
Did you mean: 

Failures on CubeMX 6.16.1 with Windows11 ARM64

SNish
Associate III

I have just spoken with an ST sidekick, and I was informed that STM32CubeMX is currently not supported on Windows ARM64.

Thank you for the clarification.

SNish_0-1769312217960.png

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Ghofrane GSOURI
ST Employee

Hello @SNish 

Actually MX 6.16.1 is supported on the following  operating systems and architectures:

• Windows® 10 32 bits (x86) or 64 bits (x64), and Windows® 11 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 42
• macOS® 15 (Sequoia), macOS® 26 (Tahoe): x86_64 and ARM-aarch64 architectures

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Ghofrane GSOURI
ST Employee

Hello @SNish 

Actually MX 6.16.1 is supported on the following  operating systems and architectures:

• Windows® 10 32 bits (x86) or 64 bits (x64), and Windows® 11 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 42
• macOS® 15 (Sequoia), macOS® 26 (Tahoe): x86_64 and ARM-aarch64 architectures

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.