cancel
Showing results for 
Search instead for 
Did you mean: 

CAN Setting Mistake in CubeMX v4.26.0

Alvin Sun
Associate
Posted on July 02, 2018 at 08:57

I am developing under STM32F4 platform. After migrating from v1.0 to v1.0 firmware, which involves a major change in CAN API, I found there's a mistake in the CubeMX CAN setting options:

The generated code relating auto retransmission changed from

hcan1.Init.NART = DISABLE;�?�?�?

to

hcan1.Init.AutoRetransmission = DISABLE;�?�?�?

However, the setting option in CubeMX is still NART, which is the inverse of Auto-Retransmission. This option name is very misleading and caused my robotics application that requires a high frequency CAN transmission fail randomly. I found this after catching a ALST (Arbitration Lost Error). Please update the cubemx software to change this setting name.

#can-bus #cubemx-4.26
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Svenn Dahlstrom
Associate III
Posted on July 16, 2018 at 09:37

I also have the same issue for L4 V1.12.0.

Please fix

Khouloud GARSI
ST Employee
Posted on July 16, 2018 at 12:00

Hello,

Thanks for your feedback! This point is under check.

If the issue is confirmed, we will update the tool ASAP.

Khouloud.

Svenn Dahlstrom
Associate III

Please fix this issue.

Just updated CubeMx to V4.27.0 and now I'm doing a project with F4 and firmware package V1.21.0 with the same issue.

This is frustrating.

Khouloud GARSI
ST Employee

Hi @Svenn Dahlstrom​ ,

Sorry for this inconvenience! The issue is confirmed and will be fixed in next releases of CubeMX.

Khouloud.

AWill.2160
Associate

Hi

As of CubeMX 5.3.0 and STM32F4 1.24.1, the issue is not fixed yet. Is it still planned to be fixed?

And if it is fixed, will we have to change again the setting of will be kept accross correctly?

Khouloud ZEMMELI
ST Employee

​Hello @AWill.2160​ ,

Could you please try with the 5.4.0 CubeMX version?

Best Regards,

Khouloud.